Posted on March 26, 2015 at 16:33Thomas,
The maximum functional operational voltage is 3.0V. Running the device at higher voltage is not suggested. It will not operate according to the specified operation parameters. The absolute maximum value for the supply voltage indicates the limit at which supplying a voltage above that limit (3.6V) may cause damage to the part.
Ken W @ST