MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3DH read zero axis ???

Posted on May 27, 2015 at 15:54HiI have a weird problem.I manufactured a PCB with to accelerometers on it. One is LIS3DH and the other if from other manufacture (ADXL346).Both works from 1.8v regulator and are connected to on the same I2C bus. Both ...

mbed Software

Posted on October 23, 2014 at 01:15I was looking for mbed resources for the F401 and VL6180 Board referenced in manual. Is that available? #vl6180x

pbeverly by Associate
  • 2086 Views
  • 5 replies
  • 0 kudos

ARHS algorithm problem

Posted on July 25, 2014 at 23:28Hello everyone,I am using iNEMO with AHRS algorithm provided by ST. I have noticed that there is a problem about function pointers initialization. These function pointers are used to point the  AHRS algorithm (whose c...

valeriagh by Associate II
  • 1295 Views
  • 2 replies
  • 0 kudos

Unable to properly initialize lis3mdl via spi and via i2c

Posted on May 13, 2015 at 11:48I am using the lis3mdl sensor with msp430 microcontroller sensor, the initial plan was to use SPI interface but it turns out the SDI pin was acting like an output pin instead of receiving data from the micro-controller...

mahlet by Associate
  • 1495 Views
  • 3 replies
  • 0 kudos

How configure lis2DH click mode

Posted on May 13, 2015 at 17:27Hi, i need to configure a lis2DH to detect tap and interrupt my micro.i cannot find any application note  about it.Please help me,thanks

MEMS microphone MP34DB01

Posted on May 09, 2014 at 17:02Hello, I'm working on mic MP34DB01. I want to use this mic with mps430 mcu. It's not clearly on datasheet, the communication protocol is SPI right ? Can the microphone triggered data? thanks #mems-microphone #mems-...

ingalbi by Associate II
  • 1400 Views
  • 4 replies
  • 0 kudos

How to calculate tilted information in LIS331DLH

Posted on May 13, 2015 at 07:34 Hi, I wish to calculate the tilted information using LIS331DLH accelerometer. I get the code to calculate tilted information when HP filter is not enabled.(I have added in this post) . when filter not...

gckk1992 by Associate
  • 816 Views
  • 0 replies
  • 0 kudos

how to estimate sound intensity using MEMS Microphone?

Posted on February 08, 2015 at 19:05hi,I've been looking for a way to estimate sound intensity using MEMS microphone for a very long time. I am using STM32F4DISCOVERY board with a MEMS microphone on it (it's MP45DT02). I wrote an application that re...

kajetan by Associate
  • 1295 Views
  • 2 replies
  • 0 kudos

Query regarding interrupt generation and acceleration values

Posted on May 12, 2015 at 12:02Hi ,we are using LIS331DLH accelerometer for our application.I have some doubts regarding acceleration values. 1) I don't get any horizontal acceleration for below configuration.        Threshold: 500mg.         Interr...

gckk1992 by Associate
  • 639 Views
  • 0 replies
  • 0 kudos

H3LIS331DL non_linearity

Posted on May 04, 2015 at 13:27I came across your portfolio for MEMS-acceleration-sensors and the H3LIS331DL suits my needs for a new developed pcb-design.I came across the non-linearity column in the data-sheet and wondered whether I understand the...