MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM303DLHC 'IR_REG_M' Registers ?

Posted on December 14, 2013 at 09:40what is the meaning of these registers? no explanation on datasheet. only that table: #msp430f5529 #i2c #lsm303dlhc #lsm303dlhc

0690X00000605UUQAY.png
eraycanli by Associate II
  • 1421 Views
  • 4 replies
  • 0 kudos

LIS3DH, x-axis is stuck with spi mode3 but working with mode1

Posted on December 28, 2015 at 06:58MCU: STM32F429NHi. I know from datasheet that spi should be configured as mode3 (CPOL=1, CPHA=1), but its working only with mode 1 (CPOL=0, CPHA=1)In mode 3 -  x-axis is stuck with value: -32624. Someone know the ...

LPS25H differential mode

Posted on August 03, 2015 at 12:37Good morning,I'm trying to set up a LPS25H sensor to read the same value as another one, which is the reference, in a controlled environment. My first guess has been to set up REF_P registers as the difference betwe...

Help with LIS2DH interrupts, novice here

Posted on December 15, 2015 at 14:07Hello,I'm reading the LIS2DH datasheet but I'm not sure of how can I do it:I've got a microcontroller connected to LIS2DH, including the INT1 and INT2 pins. I want to generate an interrupt when accelerometer detec...

Problems with LSM9DS0 I2C

Posted on December 08, 2015 at 13:54I'm using a LSM9DS0 wired to communicate with I2C. The chip seems to recognize when its being addressed, ACKs bytes, responds to reads, etc. but the problem is it always sends the same byte back. For example: I at...

vl6180x-satel

Posted on June 22, 2015 at 11:42Hello, i'am looking for a samplecode to use two vl6180x (1. satel & 2. vl6180x on the expansion shield)  on my Nucleo-Board (F401RE)? It is possible to connect two satels to the nucleo? Sincerely, Denis

dburcul by Associate
  • 1072 Views
  • 1 replies
  • 0 kudos

external clock

Posted on November 30, 2015 at 10:39hi, can someone tell me how to configure the external clock on inemo?i can see there is an oscillator on inemo, so how can i use it? thanks

mauro2 by Associate II
  • 579 Views
  • 0 replies
  • 0 kudos

inemo tutorial

Posted on November 24, 2015 at 12:17Hi, i'm trying to develop a simple application with steval-mki121v1 , the inemo board. I just want to acquire data and blink a led using a GPIO, fixed a threshold.Can someone tell me if there is a guide to begin t...

mauro2 by Associate II
  • 727 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.