Skip to main content
andrea6388
Associate II
August 3, 2015
Question

LPS25H differential mode

  • August 3, 2015
  • 4 replies
  • 917 views
Posted on August 03, 2015 at 12:37

Good morning,

I'm trying to set up a LPS25H sensor to read the same value as another one, which is the reference, in a controlled environment. 

My first guess has been to set up REF_P registers as the difference between readings from the 2 sensors which is initially stored by firmware.

I set up REF_P registers, I enable the DIFF_EN bit in CTRL_REG1 (while sensor is disabled) and finally I enable the sensor again.

The problem is that measures coming from sensors still differ for the same amount of pressure,  while if I subtract the previously evaluated difference by firmware readings are very near.

Could someone please describe the correct procedure to setup differential mode?

Thank you,

Andrea

This topic has been closed for replies.

4 replies

Nickname3482_O
ST Employee
August 5, 2015
Posted on August 05, 2015 at 15:23

Hello Andrea,

after DIFF_EN you should enable AUTO_ZERO, then set your REF_P and

run your measurement.

AUTO_ZERO gets enabled setting writing 1 into bit 1 of CTRL_REG2 (at address 0x21).

Best Regards,

Adalberto

andrea6388
Associate II
August 5, 2015
Posted on August 05, 2015 at 16:49

Thank you Adalberto,

as soon as possible I'll check the procedure.

Andrea

pfeiferm
Visitor II
December 20, 2015
Posted on December 21, 2015 at 00:51

Hello,

I have a similar problem. I'm trying to use the LPS25HB pressure-sensor sensor in differential mode with my own settings in the REF_P registers. As Adalberto suggested, I tried to first enable DIFF_EN, than AUTOZERO and after that setting the REF_P registers. But it seems that my settings of REF_P are irgnored and only the auto-copy-values form the AUTOZERO-enable are stored, because the sensor-output is always around 0 afterwards (independent of which value I've written in REF_P).

Am I doing something wrong? Or is there an other solution for that?

Andrea, did you solve your problem?

Thank you,

Marc

Nickname3482_O
ST Employee
December 22, 2015
Posted on December 22, 2015 at 19:31

Hello Marc,

proceeding step by step : first set DIFF_EN bit then enable your sensor with a given

ODR, at this point you will see ordinary measurements. Next set AUTOZERO, if everything

is correct this is the point where you will see an allmost 0 ouput as consequence of initial

pressure value being automatically copied in REF_P registers. Only after you get here REF_P

registers can be overwritten with a value of you own choice.

Regards,

Adalberto