MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPS22HB Device Independent Drivers

Posted on April 22, 2016 at 20:13I am unable to locate the platform independent device driver for LPS22HB.  Has anyone been able to locate it?I expected a link/download to be located here:https://my2.st.com/content/my_st_com/en/products/embedded-sof...

the1engr by Associate II
  • 929 Views
  • 3 replies
  • 0 kudos

Question for INEMO_PI3P

Posted on April 19, 2016 at 18:40Hi,I bought STEVAL-MKl109V2 and STEVAL-MKL159V1. But I can't find the iNEMO PI3P.Could you give me a link to download the INEMO_PI3P library.Thanks,Alex #inemo

yifeng by Associate
  • 499 Views
  • 0 replies
  • 0 kudos

LIS2DH12 INT1 open-drain?

Posted on April 15, 2016 at 19:22Is the INT1 pin of LIS2DH12 set to push-pull configuration per default? And if so, is it possible to set it to open-drain? Note: I already set the INT1 to active-low - but open-drain would be necessary as well...

christof by Associate
  • 540 Views
  • 0 replies
  • 0 kudos

LIS331DLHTR Self test failiin

Posted on April 14, 2016 at 13:15Hello, I need info about the LIS331DLHTR selftest process.The current ranges mentioned are in LSb ,which i suppose are ADC counts. i try to compute the self test ranges for x,y,z  by using self_val(selftest enabled) ...

LIS3DH resonance frequency

Posted on April 14, 2016 at 09:46Hi everybody, I'm using LIS3DH accelerometer and I need to know its resonance frequency. I did not find this information in the datasheet. Thanks in advance. #lis3dh-resonance

massimo2 by Associate II
  • 450 Views
  • 0 replies
  • 0 kudos

Need right suggestion for Acceleration/Vibration Sensor

Posted on April 09, 2016 at 11:35Dear All,I want to design sensor which use for ''Structural Health monitoring'' of Building and Bridges.I am new and searching for same but not find good resource/ans.Please guide me to select right STElectronics's M...

bhavdipm by Associate
  • 476 Views
  • 0 replies
  • 0 kudos

problem with read and write with LSM9DS0

Posted on April 07, 2016 at 15:40Hi i do the interface of LSM9DS0 using I2C interface(100khz & 400khz) but i can't read & write so am facing problem.can anyone suggest me the solution.

bhavin by Associate II
  • 530 Views
  • 0 replies
  • 0 kudos

LPS25HB questions

Posted on April 06, 2016 at 15:52Hello, new in this pressure are, for absolute pressure measurement. is the LPS25HB in free air will give 760hpar reading? for example, if I put it in a flat balloon, the reading will be 760hpar, if I start to blow...

dsun1 by Associate
  • 635 Views
  • 1 replies
  • 0 kudos

VL6180X Sub-mm Output

Posted on April 04, 2016 at 17:31Hello, The core of my questions is how would I get a sub-mm output from this sensor? All output I have come across have been to 1mm so is this an inherent characteristic of the sensor or is it rounded? If it is round...

sce by Associate
  • 514 Views
  • 0 replies
  • 0 kudos

LSM303D Magnetic interrupt mechanism

Posted on April 02, 2016 at 14:33Hi all!I've been testing for a few days the behaviour of the magnetic sensor and its interrupt capabilities. Offset registers simply are subtracted to the magnetic field measured on all of three axis and threshold re...