MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

iNemo (LSM6DS3) with external trigger

Posted on January 09, 2017 at 10:41I would like to use an iNemo with an external magnetometer (i.e. Sensor Hub mode) to gather data and place acc, gyr and mag readings in the FIFO. Is it possible to have the mag drive the ODR of the iNemo with its d...

H3LIS331DL Threshold interrupt

Posted on January 12, 2017 at 17:10Hello,I have troubles setting the H3LIS331DL accelerometer to trigger an interrupt when a programmed threshold is crossed. I can configure the device to trigger an interrupt when new data is ready on both INT1 and ...

Angular accelerometer from Gyroscope

Posted on December 24, 2016 at 13:34Hi.I need an MEMS Angular accelerometer for my application (quatrotor).As i detected in http://www.st.com/content/st_com/en/products/mems-and-sensors/gyroscopes.html?querycriteria=productId=SC1288 , ST’s gyros m...

joe ted by Associate II
  • 2927 Views
  • 6 replies
  • 0 kudos

VL53L0X not soldering all GND pins

Posted on January 13, 2017 at 10:13Hi, I am considering mounting <LINK NO LONGER ACTIVE> on the edge of a PCB on a upcoming product to save space.This would result in PIN 6 and 12 not beeing soldered to GND, what implications would this have?

Glitches with the LSM303DLHC

Posted on January 12, 2017 at 12:50I am using the magnetometer on this device, running at the max ODR of 220Hz. There are occasional (several times a minute) glitches which have the following charateristics:1. The interrupt is significantly delayed....

0690X000006062MQAQ.png

LSM9DS1TR gravity expected output

Posted on January 11, 2017 at 12:27Hi, I am using a LSM9DS1TR, with accelerometer scale set to +-16G.With the device motionless on a table, I read a decimal value of 1360 for the Z axis, and if I flip the board over I read -1360 (give or take a few ...

arthur by Associate
  • 825 Views
  • 1 replies
  • 0 kudos

X-NUCLEO-CCA02M1 Expansion sample program problem

Posted on January 08, 2017 at 07:42I have got a strange problem with X-NUCLEO-CCA02M1 expansion board interfacing with NUCLEO-L476RG. I have followedhttps://my.st.com/content/ccc/resource/sales_and_marketing/presentation/product_presentation/d3/44/d...

LIS2DH12 Double Click Interrupt

Posted on January 04, 2017 at 18:13Hi AllI am having some difficulties in configuring the Double Click Interrupt on the LIS2DH12.After power up, I am doing the following:TEMP_CFG_REG = 0xC0CTRL_REG4 = 0x80CTRL_REG1 = 0x77The above seems to work and ...

LSM6DS3 android drivers

Posted on January 09, 2017 at 11:06oliverbeirne‌Where can I find drivers for LSM6DS3 which can be used with Android 6. Android requires both drivers and HAL. I could not find anything on this site. I had seen  a github repository with ST drivers, ...

Simulation files for LPS22/25/331

Posted on January 05, 2017 at 00:51Are there any spice or cadence files to simulate the lps22h/25h/331ap pressure sensors to co-simulate them with an ASIC?If yes, how does one access them?Thanks