MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MEMS base capacitive moisture senor

Posted on March 17, 2017 at 11:24I am Designing a MEMS base capacitive moisture senor and now i am stuck with the design of inter digital electrodes (number of electrodes , width,length,gap between the fringes)

Question about LSM303AGR resolution

Posted on October 04, 2016 at 15:22Hi.I'm testing LSM303AGR. If I put my sensor module on the my desk, Z value of accelerometer's output is about 1400 LSB. I'm using high resolution mode(12bit) and 16g range. If I calculate this value as mg unit, th...

daekeun by Associate II
  • 1039 Views
  • 1 replies
  • 0 kudos

LIS2DH12 internal temperature sensor

Posted on March 15, 2017 at 11:21Hello,In my application I use a SAFT lithium battery (LS 26500). I'd like to detect it's end of live by measuring voltage value. The voltage value depends on current and temperature.So, I'd like read the temperature ...

LSM9DS0 and LSM9DS1 acceleration sensitivity confusion

Posted on March 13, 2017 at 01:49All the sensitivity values for the acceleration fit within 16 bits, however  �16 g does not.Let�s use FS �2 g as an example sensitivity level.  As the range is -2 to +2, this would be a total of 4g.  Or 4,000 Milli-G...

0690X00000606XUQAY.png

VL53L0X Performance Under Sunlight

Posted on March 13, 2017 at 07:59We have installed the VL53L0X onto one of our drones and noticed that the sensor will give 8191 or 8192 in millimeters for range measurements frequently when the drone is placed outdoors. The actual height informatio...

Gyroscope for tunneling machine

Posted on October 13, 2016 at 12:48Hello all,We are planning to include a PCB in a little tunneling machine in order to measure inclination and deviation (in degrees) in relation to an origin (0,0,0). We are looking for a sensor, maybe a gyroscope, ...

LIS2DH2 setup registers

Posted on March 09, 2017 at 20:13Hi fellows,on setting up an LIS2DH12 I wonder what settings to use for those registers:CTRL_REG2:HPCF1/2: couldn't find this in the datasheet...CTRL_REG5:How shall I enter '- -' ?And what's gonna happen with D4D_INT1...

STSW-IMG003

Posted on November 12, 2016 at 20:14Hello, currently I can't download the API STSW-IMG003. Indeed when I choose get software ==> download, I'm rediricted towards the home page: https://my.st.com/content/my_st_com/en.html#.What about this issue ? Som...