Posted on November 23, 2017 at 13:07
Hi, we are upgrading our product from a LSM9DS0 to a LSM9DS1.
During testing, we are unable to get tilt compensation working with the compass on the LSM9DS1.
We have calibrated the compass.
When using...
Posted on April 11, 2017 at 08:08
We are upgrading our IMU from a LSM9DS0 to LSM9DS1. However we are having issues with the magnetometer on the LSM9DS1. Even after min/max calibration it doesn't appear to give correct heading.
We are aware tha...
Posted on March 13, 2017 at 01:49All the sensitivity values for the acceleration fit within 16 bits, however �16 g does not.Let�s use FS �2 g as an example sensitivity level. As the range is -2 to +2, this would be a total of 4g. Or 4,000 Milli-G...
Posted on November 23, 2017 at 15:02Thanks for responding.I have hard iron calibration applied to the LSM9DS1I did look at that. The Pin 1 indicator is also in a different position in the images which makes it hard to work out what has changed.I qui...