MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LIS3MDL data interpretation

Posted on May 15, 2017 at 18:45Hello,I have the a question about LIS3MDL.I have read http://www.st.com/resource/en/datasheet/lis3mdl.pdf and an http://www.st.com/resource/en/application_note/dm00136626.pdf, but have no idea, how to interpret the dat...

LSM6DS3 linker error L6218E - LSM6DS3_IO_Read

Posted on May 09, 2017 at 11:39I am getting a linker error L6218E when compiling code for the LSM6DS3 Gyroscope. The error points to the LSM6DS3_IO_Read and LSM6DS3_IO_Write functions. These have been declared and are to be imported but there is no ...

daithi62 by Associate II
  • 1634 Views
  • 3 replies
  • 0 kudos

LIS3DH Click Interrupt

Posted on May 15, 2017 at 10:32Hey guys, I dunno what I add but seems I can't generate interrupt after I click on LIS3DH, here what I do.void Acc__EnableClickDetect(void){  LIS3DH_SetAxis(LIS3DH_X_ENABLE  |LIS3DH_Y_ENABLE | LIS3DH_Z_ENABLE );  LIS3D...

X-NUCLEO-CCA02M1Evaluation program not recognized

Posted on May 14, 2017 at 23:18Hello,I want to test the sample application. I can compel and load from uVision whithout problem.I connect a second USB cable  on the X-NUCLEO-CCA02M1 but the board is not recognized on my PC under Win 10. Thanks for y...

LSM303AGR question

Posted on May 12, 2017 at 09:29       1.当å‰�的库ç£�力计使ç�?¨äº†SWUå��标系,这个时候ç£�力计芯片的那个方å�‘指å�‘æ­£å�—.2.ç£�力计校准是通过函数(osx_)è¿�?回为1表示校准æˆ�功。我们怎么验è¯�这个校准å�Žçš„...

LIS3DH Accelerometer Click Detection

Posted on May 09, 2017 at 11:40Hey guys, I am trying to do click detection for my LIS3DH accelerometer. For single click, what I should add inside my code? Here is my code, please help me. void Acc__EnableClickDetect(void){  LIS3DH_SetAxis(LIS3DH_X_...

LSM6DS3 not reading stable value

Posted on May 11, 2017 at 05:46Hi All,I am using LSM6DS3  accelerometer and gyroscope sensor.I am interfacing with I2C. I have initialized the accelerometer register and reading the respective X,Y,Z register .I am not getting stable value. i am not ...

0690X00000605JPQAY.png

LIS3DH: What current ratings for input/output pins?

Posted on February 12, 2016 at 19:38I've checked the LIS3DH's spec sheet and I can't find specs for input or output current on its I/O pins. Somewhat difficult to design in this part when we don't know its I/O pin current source/sink specs. Are thes...

LSM9DS1 read from magnetometer problem

Posted on October 24, 2016 at 22:38Hello! I made a custom board with LSM9DS1  module on it. Pins SDO_M and SDO_A/G is tied together. I use SPI to communicate with module. When i write/read to/from accelerometer/gyroscope registers all works fine but...