MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

M24M02 I2C EEPROM Read Lock Status

Posted on February 16, 2017 at 15:48I am looking at the data sheet for the M24M02 and I want to read the Lock Status.  The data sheet says thisThe locked/unlocked status of the Identification page can be checked by transmitting a specific truncated ...

ttatakis by Associate III
  • 729 Views
  • 1 replies
  • 0 kudos

LPS25HB questions

Posted on February 14, 2017 at 23:24We are evaluating the LPS25HB BP sensor, and have a couple of questions. I notice that several forum members have asked similar questions, but without receiving a reply. I would really appreciate an answer, as thi...

John L by Associate
  • 1488 Views
  • 3 replies
  • 0 kudos

LIS2DH12

Posted on February 14, 2017 at 13:03Hi all,I have got a technical question, if is possible to get some helpful feedback, I would really appreciate it, please.I have recently purchased a LIS2DH12 accelerometer and I am plugin it within a Teensy modul...

LSM9DS1.....Can someone please explain DEN_A/G pin? The datasheet mentions this pin once and does NOT explain whether it should be driven by host or not.

Posted on February 10, 2017 at 20:05The LSM9DS1 datasheet does not give a good description of the DEN_A/G pin.  Can someone add value to this?  Should it just be pulled high and never toggled by MCU?  Reference schematics of part from Sparkfun, etc....

swenner by Associate
  • 623 Views
  • 1 replies
  • 0 kudos

WESU1 Clock Configuration issue

Posted on December 20, 2016 at 15:52hi all,     I have recently purchase a WESU1 device and used it as a reference for my custom wearable device design. i re flashed the WESU1 device with the sensor example firmware(STSW-WESU1) found it from followi...

LSM303D Interrupt

Posted on December 01, 2016 at 12:40I am having trouble getting the click interrupts to work for the LSM303D. using the library provided by Pololu for arduino I can get this code working for the DLHC[code]#include <Wire.h>#include <LSM303.h>long thi...

MP34DT01 sensitivity for far-field application

Posted on October 06, 2014 at 20:30Hello, I would like to prototype a conference room microphone. Is the MP34DT01 mic able to capture sound from a human speaker away from 3 or 4 meters ? (ex: classroom) If no, what would be the recommended mic ? In ...

pierre by Associate
  • 741 Views
  • 1 replies
  • 0 kudos

Resolved! How to configure LIS2DE12 to support ODR=5.3kHz ?

Posted on December 13, 2016 at 01:06Hi All, I am developing device to analyze vibration with LIS2DE12 acceclerometer.I have encountered problem that sensor did not work with ORD=5.3kHz, it worked fine for all other ODRs.How to configure sensor to wo...

q.lsm6ds3 anti-aliasing filter order

Posted on May 09, 2016 at 13:05hi, I've got a few questions. 1. what is the order anti-aliasing filter of the Acc? 2. what is the order anti-aliasing filter of the Gyro? 3. how does the DLPF1 filter help me if the cut-off freq is higher then nyquist...

amir5 by Associate
  • 921 Views
  • 3 replies
  • 0 kudos