MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM9DS1 SPI only write

Posted on March 24, 2017 at 11:48What is the meaningful of 'SPI only write' SIM bit of CTRL_REG3_M (22h) register?How magnetometer values can be read if SPI is in write only mode?

Mich1 by Associate III
  • 601 Views
  • 1 replies
  • 0 kudos

LSM303AGR accelerometer readings problem

Posted on April 19, 2017 at 14:25Hi all,I'm trying to interface a LSM303AGR, to get the magnetometer and accelerometer values in I2C.The component is responding well to whoami requests (both compass and magnetometer parts), I manage to get mag value...

LSM6DS3 Delay

Posted on April 19, 2017 at 23:28I'm using the LSM6DS3 to control a gimbal with a camera on it, and I'm noticing that my control is suffering due to delay in the system. I have configured the LSM6DS3 for an output datarate of 208Hz, with the fifo in...

Konami by Senior II
  • 454 Views
  • 0 replies
  • 0 kudos

''nano'' vs ''pico'' vs ''femto'' accelerometers?

Posted on April 13, 2017 at 13:39Totally new to ST accelerometers, I can see that they're grouped into what look like three 'families' -- nano, pico and femto. Is there a short explanation of the differences between those three families? A link to a...

Rob Day by Associate
  • 2377 Views
  • 2 replies
  • 0 kudos

LPS25HB temperature difference?

Posted on October 18, 2016 at 09:49Hi!The HTS221 sensor and LPS25HB pressure sensor are together in the development board. The temperature difference between the output of the two sensors too high. HTS221 temperature value is close to the actual tem...

ksw280 by Associate
  • 750 Views
  • 3 replies
  • 0 kudos

LIS3DH: XYZDA on INT1 doesn't clear reliably

Posted on April 18, 2017 at 07:48I'm using an LIS3DH accelerometer. It is configuring properly and returning valid data when manually read at a fixed interval. Now I'm trying to switch to the use of its XYZDA signal that is emitted on INT1.I have al...

IIS2DH Reading FIFO

Posted on April 13, 2017 at 01:08With a 2g scale sampling @25Hz the FIFO fills with data and I am reading the contents up to the watermark. HR and LPen are disabled.With the Z-Axis pointing toward earth I get the following data for the X-Axis using ...

LSM303DLHC DRDY Behaviour

Posted on April 13, 2017 at 12:58The detailed behaviour of the LSM303DLHC DRDY pin (pin 9) is not elaborated upon in the datasheet.We have observed that it generates active low pulse but this is not detailed in the datasheet. What are the timing req...

tom2399 by Associate
  • 593 Views
  • 1 replies
  • 0 kudos

IIS2DH Reading and Clearing FIFO

Posted on April 12, 2017 at 17:13I am moving to the IIS2DH from the LIS3DSH because it is end of life. I am having an issue with reading the FIFO. I can enable FIFO mode and it seems to fill and generate an interrupt on OVRN and WTM just fine, but t...

Magnetometer difference between LSM9DS0 and LSM9DS1

Posted on April 11, 2017 at 08:08 We are upgrading our IMU from a LSM9DS0 to LSM9DS1. However we are having issues with the magnetometer on the LSM9DS1. Even after min/max calibration it doesn't appear to give correct heading. We are aware tha...