MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MEMS-Sensors with STM32F4 Discovery

Posted on June 13, 2017 at 22:19Hello everybody, I am a student and I really don't have a clue how to program an uController. This year we have a big project with a STM32F4 Discovery board. We need to read the data from an additional board, that inc...

LSM6DSM Latency and Detailed Model

Posted on October 18, 2017 at 13:51Hello everyone,I am using LSM6DSM in a optical stabilization system. And I would like to construct detailed sensor model. On the datasheet, there is a diagram which shows gyro output structure roughly. Sensor laten...

IKS01A2 register read help

Posted on October 19, 2017 at 10:14Hello, my name is Domenico, I'm a mechanical engineer and I am working on a standalone vehicle dynamic model for my master thesis using STM32F401RE board + IKS01A2 shield. I am new to hardware programming so I'm ex...

''gcc'' not found in PATH

Posted on October 17, 2017 at 23:12I am trying the 'STM32CubeExpansion_BLE1_V3.2.0' to build the BLE expansion board However I got the build error for project :STM32CubeExpansion_BLE1_V3.2.0\Projects\Multi\Applications\SensorDemo\SW4STM32\STM32F401R...

LIS3DSH vector filter

Posted on October 12, 2017 at 08:44Hi, I wanted to used internal filter of the accelerometer LIS3DSH, but I couldn't find proper documentation regarding this. Can anyone please help me regarding this. 

Resolved! LIS2HH12 : FIFO multiple reads (burst)

Posted on October 13, 2017 at 17:25According to chapter 5.3.8 in LIS2HH12 http://www.st.com/content/ccc/resource/technical/document/datasheet/c9/16/f2/79/ca/31/47/89/DM00096789.pdf/files/DM00096789.pdf/jcr:content/translations/en.DM00096789.pdf, mul...

LSM9DS1 Temperature Drift Characteristics

Posted on October 13, 2017 at 17:32Hello,I am looking through the datasheet for the LSM9DS1 and I do not see temp drift figures for the accelerometer or gyroscope.  I would expect to see some number in LSB/degC and I see nothing.  What is the accele...

LSM303D Self-test did not function normally when VDD=3.3V

Posted on October 15, 2017 at 05:21Hi,   In out production process, the self-test function of LSM303D was taken to perform product testing. The Self-test was always OK when VDD was about 2.7V. However, we found that when the VDD was set to 3.3V, som...

looeyc by Associate II
  • 1098 Views
  • 1 replies
  • 0 kudos

Modifying the API of the VL53L0X for use with other uCs

Posted on September 21, 2016 at 16:19Hello, I have some questions to the developers of the API of the VL53L0X (Help from fellow users of this sensor is also highly appreciated). In the next paragraph you find the text which I already shared with cus...