MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

lsm6ds3

Posted on December 12, 2016 at 14:48We need Linux device drivers of lsm6ds3 for kernel 3.7.6.Can somebody provide drivers

Does ST have plan to make SPI version of VL53L0x?

Posted on January 20, 2017 at 06:43I wonder that ST has plan to make another enhanced version of VL53L0x.VL53L0x's I2C speed and output rate is slow.If a spi interfaced device is made, I hope that it would support the daisy chain.Currently multiple ...

just4you by Associate II
  • 693 Views
  • 1 replies
  • 0 kudos

LIS3DH SPI pull-up values?

Posted on December 19, 2013 at 17:28In LIS3DH datasheet (Doc ID 17530) on figure 3 page 12/42 we can see: ''When no communication is on-going, data on CS, SPC, SDI and SDO are driven by internal pull-up resistors.'' What is the pull-up value? Are t...

Mich1 by Associate III
  • 611 Views
  • 3 replies
  • 0 kudos

H3LIS200DL Readings and Conversion

Posted on June 13, 2017 at 06:03Hello:I am getting some bizarre values from this device, and maybe it's not configured correctly, or I am not reading it correctly.It appears I can send and read from the device. I can use the 'WHO_AM_I' and get back ...

LSM9DS1 Gyroscope does not work?

Posted on June 08, 2017 at 16:57Hi all,I am testing a LSM9DS1 module to replace a L3GD20. I get readouts for the gyro, the accellerometer and the magnetometer. However when I turn my pcb I can see value changes on the accellerometer and the magnetom...

0690X00000603rqQAA.jpg

lis3mdl vs lsm9ds0

Posted on June 12, 2017 at 20:42Hi,Some time ago I've succesfuly used lsm9ds0 (SparkFun) for 3D magnetic field readings. Today I'm trying to upgrade my device to use lis3mdl (MinIMU-9 v5 Gyro) but the magnetometer output is different than lsm and I ...

LIS2DH12 Measure conversion

Posted on June 06, 2017 at 09:20I am having some problems when I try to get data from my sensor. I can read registers and get some data but I don't know how I should do the covnersion to get a real value.I am using an arduino and I found some librar...

P M by Associate III
  • 1920 Views
  • 10 replies
  • 0 kudos

LIS2DH12 - the frequency tolerance of data rate (ODR)?

Posted on June 08, 2017 at 11:05Hello,I set the data rate (ODR) to 400Hz in high resolution mode with fifo stream mode enable of LIS2SH12.For 3 minutes measurement test, I excepted to receive 72000 (400 * 60 * 3) data for each axis, however I only r...