MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Solution versus ADXL203

Posted on July 23, 2014 at 16:56I am looking for the best option versus this ADI part. Key requirements are - powered by 3.6V DC.- zero g temperature stability of 0.1 mg/C or better.- resolve angles down to 0.5 degrees at least, 0.1 degrees preferre...

PI3P on M1 module??

Posted on July 21, 2014 at 18:30I wanted too know if it is possible to use the pro version of the engine on the M1 module, is the hw compatible?Thanks for the help

franz by Associate
  • 733 Views
  • 0 replies
  • 0 kudos

H3LIS331DL 3-wire SPI

Posted on July 20, 2014 at 11:01H3LIS331DL accelerometer has 3-wire SPI mode. What i will get in this (3-wire) mode at pin number 7 (SDO in 4-wire mode). Is it pull down, pull up or open drain ?

tomasz by Associate
  • 877 Views
  • 0 replies
  • 0 kudos

Looking for EK3LV02DQ - Eval Kit software

Posted on July 19, 2014 at 15:18Transferring my life to a new machine and can't find the mini-CD that came with this eval kit.Does anyone know if it's available online and where?Thanks,Geoff #accelerometer

geoff by Associate
  • 776 Views
  • 0 replies
  • 0 kudos

Function INEMO2_SDK_Connect

Posted on June 29, 2014 at 17:20Morning, everyone,I used a demonstration board STEVAL-MKI062V2. I wrote a small C++ program and want to get data from the sensor. It looks like, that some functions are not in the dll file (''iNEMO2_SDK.dll'') .The co...

s_wd8y9x by Associate
  • 1076 Views
  • 1 replies
  • 0 kudos

LIS3DH detect position away from a zone

Posted on July 16, 2014 at 11:59Dear all,I'd like to configure the LIS3DH in order to enter my uc in sleep mode in a certain position P0 and then be awaken when the position move from P0 +/- threshold.I dont want to detect a movement but a position ...

LIS3DH Click Interrupt

Posted on March 25, 2014 at 22:50The data sheet makes no explicit mention of a way to force this interrupt to latch and clear when the CLICK_SRC register is read (like the INT1_CFG registers can).App note AN3308 states that this behavior can be achi...

jose by Associate
  • 907 Views
  • 1 replies
  • 0 kudos

Inemo-M1 'LSM303DLHC_AccDataReady.c' problem

Posted on June 18, 2014 at 11:54Hi guys,I have jsut started using the Inemo_m1 discovery board.After Installing the software and doing some hello world projects (using KEIL IDE;debugged via ST-Link debugger), I decided to setup communication with th...

bouvett by Associate
  • 1800 Views
  • 3 replies
  • 0 kudos

LIS3MDL reboot memory

Posted on July 09, 2014 at 13:00CTRL_REG2 contain REBOOT bit - ''Reboot memory content''. Which memory this bit reboots?A found only one memory - non-volatile memory trimming values ofsensitivity (So) and Zero-gauss level (TyOff). If I can reboot th...