MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to activate Sensor Hub mode in LSM6DSL

Posted on August 23, 2017 at 16:50Hi!, I'm trying to do bring-up of a board that has the LSM6DSL and other sensors in its sensor hub. I can read and write to other registers except for CTRL10_C (19h) and MASTER_CONFIG (1Ah) which I can only read and...

LIS2DW12 SA0 Pull-Up

Posted on August 24, 2017 at 11:14I have a design in which I have to put the line from SA0 to GND (this is mandatory since the alternate I2C address is already used on my I2C bus). However, the internal pull-up of SA0 seems like it can not be disabl...

HTS221

Posted on August 23, 2017 at 14:55Register 0x2A and 0x2B are aways fixed when I read back register even with restarting the sensor power.Config before reading back register:Register_0x20=0x83: (active mode, continuous update, output data rate: 12.5H...

Difficulty Putting LSM303AGR to Sleep

Posted on August 01, 2017 at 20:37Hello,I am attempting to integrate the https://community.st.com/tags♯/?tags=lsm303agr into an existing product and I am having difficulties bringing down the power consumption of the LSM303AGR to reasonable levels. ...

Axis X is not changing

Posted on August 14, 2017 at 17:33Hi,I'm using LSM6DSL and unable to operate X axis on accelerometer. The Y and Z axes give me the right results but X axis is stable at 32756 and changes only by 5 points. I have 4 devices with LSM6DSL and all behave...

LIS3MDL availability

Posted on February 15, 2017 at 10:12We're trying to get some LIS3MDL parts for some sample boards we are making. Seems there is no supply anywhere. Does anyone know what the problem is, or when it's likely to be sorted? Better still: any ideas where...

LSM9DS1 Accelerometer Calibration required?

Posted on May 01, 2017 at 18:41We are making roll measurements (atan2(ay,az)) using the LSM9DS1's accelerometer.   We see extremely little error, just fractions of a degree.  Since this is within our required accuracy, we are thinking that we don't ...

djacobs by Associate
  • 1283 Views
  • 3 replies
  • 0 kudos

Fielf of view of VL53LOX

Posted on September 29, 2016 at 13:03How the 25 degree field of view of VL53LOX TOF sensor was covered? If there any algorithm to measure the distance with in that field of view ?

VL6180X addressing multiple sensors

Posted on July 23, 2017 at 16:03I am working with the VL6180x and I would like to connect multiple sensors via an expansion board by ST (*). Therefore I want to communicate to single sensors, so I have to change each single I2C-Device-Address via th...

STEVAL-WESU 1 Accelerometer reports 0 data

Posted on August 16, 2017 at 11:52The accelerometer on my STEVAL-WESU1 has stopped reporting data. For instance, in the Plot data demo, I can see:Data: X: 0  Y: 0  Z: 0After I charge it, it does report some data but only for some seconds.I can see t...