MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM303D Self-test did not function normally when VDD=3.3V

Posted on October 15, 2017 at 05:21Hi,   In out production process, the self-test function of LSM303D was taken to perform product testing. The Self-test was always OK when VDD was about 2.7V. However, we found that when the VDD was set to 3.3V, som...

looeyc by Associate II
  • 663 Views
  • 1 replies
  • 0 kudos

Modifying the API of the VL53L0X for use with other uCs

Posted on September 21, 2016 at 16:19Hello, I have some questions to the developers of the API of the VL53L0X (Help from fellow users of this sensor is also highly appreciated). In the next paragraph you find the text which I already shared with cus...

Resolved! Do the LSM303AGR CS lines have internal pull-downs?

Posted on October 10, 2017 at 21:50 Do CS_XL and CS_MAG have an internal pulldown so if they are left floating there are no issues?Will it hurt the part if INT_1_XL and INT_2_XL are connected to 0V as long as we don�t try to use them? What happe...

0690X00000608YjQAI.png

The fluctuation in the readings from a LIS3MDL sensor

Posted on October 11, 2017 at 11:12 I'm testing a LIS3MDL magnetic field sensor using an Arduino Pro mini.The Arduino IDE has a library for Pololu LIS3MDL module and example codes as well. I connected the sensor module to the Arduino via I2C and ...

M. Jeong by Associate II
  • 751 Views
  • 1 replies
  • 0 kudos

MKI109V3 board compatibility with MKI173V1

Posted on October 11, 2017 at 02:48Hi,  my question:  Is there a specific COM driver and specific GUI revision that I must download for this to work?I recently bought a MEMS mainboard STEVAL-MKI109V3 and board for LIS2DS12 p/n MKI173V1.   Here is th...

Resolved! LIS3MDL Doesn't Respond Properly Over SPI

Posted on October 08, 2017 at 06:56I am attempting to communicate with a LIS3MDL through the SPI interface, yet I am unable to get a single, valid response back. Moreover, the responses I am getting violate the setup and hold times on the SPI interf...

0690X00000608WJQAY.png
Tim S by Associate
  • 1036 Views
  • 2 replies
  • 0 kudos

Interrupts arent working

Posted on October 10, 2017 at 15:14 i am working with the LSM9DS1.I want to read the accelerometer data using interrupts. The problem is that, when i enable the 'data ready interrupt'(INT_DRDY_XL) and read and printf STATUS_REG, to see whether one o...

AIS1120SX

Posted on October 10, 2017 at 03:45Hello,Has anyone written Arduino code (Arduino Uno with Arduino IDE) to read accelerometer values from the AIS1120SX using SPI that they are willing to share?-John

Resolved! LSM6DS33 self test

Posted on October 07, 2017 at 20:45Hello,I am using a Pololu Minimu9 v5. I successfully did a self test of the LIS3MDL 3-axis magnetometer and now I am trying to self test the LSM6DS33 with the procedure mentioned in the application note. My test ap...