MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Why is my INT1 of LIS2DW always at high?

Posted on January 25, 2018 at 18:52Hi,    My problem is I can not receive the interrupt signal of INT1 when I using FIFO mode with FIFO buffer full trigger. I find the cause is that the INT1 is always at high, but I expect it should be rise high whe...

0690X00000609UdQAI.png 0690X00000609UiQAI.png
Allen Lin by Associate II
  • 1259 Views
  • 1 replies
  • 0 kudos

LSM6DS3 Accel-Gyro Data problem

Posted on January 25, 2018 at 11:16Hi, i am using this sensor for a while now ,and i have a problem when i use together accelerometer and gyroscope. When i use them seperately everything works great, but if use both of them and acquire data from the...

Alex Dim by Associate II
  • 905 Views
  • 0 replies
  • 1 kudos

Data mismatching while Hard and soft reset

Posted on January 18, 2018 at 06:19Hello Miroslav, I have done following configuration for IIS2DH acceleromenter./////////////////////////// Sample Code ////////////////////////////////////////////////////response=LIS3DH_GetWHO_AM_I(&who_am_i); if(w...

Bluecoin microphone distances

Posted on January 24, 2018 at 11:39Hello,I have 2 questions about the microphone distance of the Bluecoin hardware.I have ordered this hardware to experiment with the microphones and the beam-forming algorithms and it works very impressive. I would ...

Marcel . by Associate
  • 796 Views
  • 0 replies
  • 0 kudos

LIS2DE12 Activity/Inactivity detection

Posted on January 22, 2018 at 17:39HelloI want to detect the movement for 10 min from an accelerometer LIS2DE12, I want to know if I can use the configuration of the interuption register or i must use a REal time counter Thanks

LSM9DS1 : How to validate IMU feature in Android

Posted on January 22, 2018 at 08:51Hi ,I am using LSM9ds1 in one of my project. The main reason for using this chip is,  it is THE one recommended for IMU feature, where all 3 sensors are in one chip.In Android 6.0 , I am getting all 3 sensors data ...

Spurious INT2 on LSM6DSMTR

Posted on January 17, 2018 at 02:13I believe I've configured my system (LSM6DSMTR connected to Nordic nRF52382 via I2C) to interrupt on INT2 when the FIFO threshold is reached.  What is happening, is that I get an interrupt when data first appears i...

LSM9DS1. DRDY_M pin

Posted on January 16, 2018 at 11:10In the datasheet say that this pin must be work(indicate moment of magnetometer new data avalaible ) automatically(without need of configuration), but it doesn't work. Why? In the http://www.st.com/resource/en/data...

can iNEMO M1 work with Nucleo board programming?

Posted on January 19, 2018 at 11:22hi everyone,i'm trying to debug my program on the iNEMO M1 but when i press the reset button to start the program the iNEMO is disconnected from the debugger and i can't talk to it anymore, so i can't see where the...