MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DE12 InActivity Interrupt

Posted on February 21, 2018 at 17:38Does the LIS2DE12 have an InActivity interrupt that can be set in a control Register. The Lis2HH12  has the InActivity interrupt which can be set in control register(0x22).  I do not want to use the Lis2HH since i...

LIS3DSH - Effective resolution calculation help

Posted on February 16, 2018 at 17:47Hi all,I'm try to understand what can be the real usable resolution of the LIS3DSH accelerometer because I need to evaluate it for inclometric measurements.From the datasheet I can read a PSD=150ug/sqrt(Hz) @ ODR=...

FF1 by Associate III
  • 1702 Views
  • 2 replies
  • 0 kudos

What is sample Period in MotionFX_Manager.h library?

Posted on February 19, 2018 at 06:16Hey,I am running a sample code for STM32L476RG-SensorTile. In the MotionFX_Manager.h library I found : #define SAMPLE_PERIOD       ((uint8_t)10)   /* [ms] */.Can any one please tell me what is this about? Is it th...

Gatt table,Sensortile

Posted on July 02, 2017 at 10:17HelloJust starting to interact with sensortile through Linux, would be very appreciated if any body could do me a favorand let me have the gatt table, uuid,etc..RegardsHesan 

MotionFX gives wrong results

Posted on February 14, 2018 at 20:16 Hello to all, I'm trying to get run the MotionFX library using STM32F4 Discovery board and STEVAL-MKI159V1 board (which consists of 9 axes LSM9DS1 inertial module). I represent this module as a combination of ...

LSM9DS1 magnetic Z axis unstable time acquisition

Posted on February 16, 2018 at 17:41hi everyone!i did this configure LSM9DS1://Magnetometer    Write1AddressMag(CTRL_REG1_M,0x70);    Write1AddressMag(CTRL_REG2_M,0x00);    Write1AddressMag(CTRL_REG3_M,0x00);    Write1AddressMag(CTRL_REG4_M,0x0c);  ...

Failed to enable interrupt mode

Posted on February 07, 2018 at 14:53Hi,I am working on some motion detection product.LIS2HH12 is chosen as the motion detector. We want to use it in interrupt mode.Unfortunately, we failed to get any signal on INT1 pin, observing by an oscilloscope....

LSM9DS1 on single SPI bus with other devices

Posted on February 15, 2018 at 15:35We need to share one SPI bus with LSM9DS1 and other devices. The problem is that when the CS signal is inactive, the chip expect I2C communication on MOSI/SDA line. What happens if there is a communication with ot...

VL53L0X inialisation failing in PerfomRefSpadManagment

Posted on October 05, 2017 at 07:00Debugging shows it fails due to error in the VL53L0X_REG_RESULT_INTERRUPT_STATUS register read in VL53L0X_GetInterruptMaskStatus.  Can anyone tell me what values 0x50, 0x54 and 0x4C describe and how to resolve it?M...