User Activity

I'm trying to get SecureBoot running on STM32MP157.After opening and reading about 30 pages of your wiki and basically following [1] I was able to create keys and convinced yocto into generating "*_Signed*" files.Sadly I then got confused with public...
 We have the STM32MP157 EV1 Board, build our own yocto images (using the st layers) and are able to flash the images into emmc using STM32_Programmer_CLI.exe. Everything works great.Now we received our first custom boards with the same STM32MP157 Chi...
We got the STM32MP157F-EV1 and struggle a bit with the understanding of OTPs. We cloned the STM32PRGFW-UTIL repository [1], put the dip switches into "forced USB boot for flashing" mode (all off) and uploaded the provided image: STM32PRGFW-UTIL\Proje...
We are using a STM32MP157A-DK1 and try to reduce power consumption.1) When A7 and M4 are running we measure around 300mA.2) When A7 is in Suspend-To-Mem and the M4 is still running we measure around 80mA.3) When the M4 also enters standby mode the po...
Posted on June 22, 2017 at 14:51We have two prototype boards each equipped with a LIS331HH.One of the sensors seems completely broken because the Z axis shows values around 2.3g while laying flat on the table. Because of that we were now looking int...
Kudos from
Kudos given to