MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unico: The adapter board has not been recognized.

Posted on April 19, 2018 at 02:10I am using a STEVAL-MKI109v2 with a STEVAL-MKI172v1 sensor board. When I run Unico 6.0.0.0 the MKI109v2 is not in the list of devices but the MKI172v1 is. When I select MKI172v1 and attempt to connect I get the follo...

spencer2 by Associate
  • 1452 Views
  • 1 replies
  • 0 kudos

Record microphone and motion sensors simultaneously

Posted on April 03, 2018 at 08:59I have a SensorTile Kit (STLKT01V1) running the http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32-ode-function-pack-sw/fp-sns-allmems1.htmlwhich I can...

LSM9DS1 Wake Up Interrupts

Posted on November 06, 2017 at 17:26The original post was too long to process during our migration. Please click on the attachment to read the original post.

Pastrana by Associate II
  • 2618 Views
  • 4 replies
  • 0 kudos

LIS2DE12 WTM signal not cleared when reading from FIFO

Posted on April 17, 2018 at 23:55Hi All,I'm using an LIS2DE12 in stream mode with the watermark set to 15 FIFO entries and with the WTM bit being driven out INT1. When INT1/WTM goes high, I read out 16 FIFO entries and, as expected, INT1/WTM goes lo...

LSM9DS1 standby consumption

Posted on April 11, 2018 at 17:33What is LSM9DS1 standby consumption (all sensors off)?The datasheet says nothing, no value in Electrical characteristics section.Its predecessor LSM9DS0 has 6uA typical.

LSM6DS3 & m24c64 power consumption high

Posted on February 01, 2018 at 16:17Hello All,We are doing a wearable product where we using LSM6DS3 & M24C64 but power consumption much high than specified.LSM6DS3 is taking around 300uA just by powering on. As we understand from datasheet by defau...

piyush by Associate
  • 1504 Views
  • 2 replies
  • 0 kudos

LIS3DH - Motion and crash detection

Posted on February 26, 2018 at 12:02Hello allMy goal is to use two INT pins to generate two interrupts in a device which will be used in a car. INT2 will be pulled when a crash of the car is detected and INT1 when the car moves.Here is my init setti...

Resolved! LIS3DH and LSM9DS1 accelerometer comparison

Posted on April 13, 2018 at 14:16Hello,I am trying to compare LIS3DH and LSM9DS1 (accelerometer part) and I am suprised by the result:The LIS3DH has the configuration: CTRL1: 0x67 (ODR = 200Hz, LPen=0, ) CTRL4: 0xA8 (BDU, 8g, HR)   => sampling frequ...

0690X00000604aSQAQ.jpg
Mich1 by Associate III
  • 1282 Views
  • 2 replies
  • 0 kudos

LISD2E12 INT1_THS not changing tilt threshold

Posted on February 23, 2018 at 21:28 The INT1_THS register value does not seem to change the threshold at which an event is triggered. I can read and write the INT1_THS(0x32) so I know my writes are working. I poll the INT1_SRC register and watch t...