MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Interrupt and FIFO settings in ISM330DLC

Posted on April 27, 2018 at 09:15Please tell me the details on Interrupt and FIFO settings in ISM330DLC. I need to store the Gyroscope and Accelerometer data into the FIFO . Please tell me what changes i need to do in kernel source code of ism330dlc...

shammi d by Associate II
  • 890 Views
  • 0 replies
  • 0 kudos

Resolved! LIS2DH12 excessive current draw

Posted on April 16, 2018 at 12:37I am using LIS2DH12 on my custom designed board for a BLE application. I noticed that the PCB had a huge current draw than expected and on further digging found the accelerometer to be drawing the excessive current w...

How to upgrade firmware for STEVAL-MKI109V3?

Posted on April 23, 2018 at 21:33Hi, I downloaded the Unico 6.0.0.0 and selected the STEVAL-MKI179V1 for LIS2DW12 sensor. I am using the motherboard STEVAL-MKI109V3 and i getting the same error. How to solve firmware issue for this motherboard?I hav...

0690X0000060AilQAE.png

Configure interrupt for LIS2DH12

Posted on April 24, 2018 at 17:11I am trying to configure an interrupt on a LIS2DH12 in order to detect when the device is being hit.I tried just configuring one axes to generate the interrupt. But Interrupt is never being fired (Or it is fired cons...

P M by Associate III
  • 831 Views
  • 0 replies
  • 0 kudos

MotionFX and rotation_9X

Posted on April 24, 2018 at 13:34Hello to allI'm trying to use MotionFX sensor fusion library in my application with STM32F4.It seems to me that the 9X mode works good enough. But I'm confused about my results during sensor rotation around 3 axis:1)...

How to add STEVAL-MKI179V1 into Unico device list

Posted on November 10, 2017 at 09:57when i use STMicro motherboard STEVAL-MKI109V3 to evaluate the MEMS sensor board STEVAL-MKI136V1 and STEVAL-MKI179V1, found some problems.1. I can not find the STEVAL-MKI179V1 in the device list of Unico.    How t...

_legacyfs_online_stmicro_images_0690X0000060MvQQAU.png _legacyfs_online_stmicro_images_0690X0000060MvfQAE.png

Cann't complie to eMotionV2_REL_5.0.0.zip(in en.stsw-mki109w.zip)?

Posted on April 24, 2018 at 10:31Hi..I use STEVAL-MKI109V2(Demo board) and MKI160V1(sensor).and i use IAR Embedded Workbench V7.20 Version..so when i open to project file,comming message like this..'Broken options were detected in the project file A...

sw lee by Associate II
  • 746 Views
  • 0 replies
  • 0 kudos

Cann't complie to eMotionV2_REL_5.0.0.zip(in en.stsw-mki109w.zip)?

Posted on April 24, 2018 at 10:20Hi..i use steval-mki1092V2(demo board) with mki160V1(sensor)..so i was download to en.stsw-mki109w.zip(for Windows) file...and  i use to IAR Embeded Work...7.20 Version...so when i open project file,come to msg like ...

sw lee by Associate II
  • 734 Views
  • 0 replies
  • 0 kudos

LPS33HW - false reading both pressure and temp

Posted on April 03, 2018 at 00:53Hi guys,I have STEVAL-MKI183V1 connected to stm32l476rg NUCLEO. I have downloaded the C example code. Setup the SPI and the Interrupt pin using STM32CubeMX. With the help of some example code i hooked it all up. I ge...

0690X0000060AMaQAM.png 0690X0000060AJXQA2.png