User Activity

Hello all,I have developed a custom control board and a custom power board. I am trying to add them to MotorControl Workbench 6.1.1 and I have written a custom JSON files describing both board. A few interesting things:I am using STM32G431RBT6 as my ...
Hi every one. I have made a HID + CDC USB composite device. Windows recognizes it and I can control the volume and I have a COM port. HID is interface 0 and the CDC is interface 2 if this is of any significance. I can open the COM port with Tera Term...
Hello everyoneHow do I draw a line using code. For example I receive over UART a number and I need to draw lines on my screen. Start and end positions are unknown also is the number of lines. until I know the user input So I need to draw a few lines...
Hello all,I have written a External Loader using nucleo-l476rg and S25FL127 16mb NOR flash using 64k sectors. I was using it with TouchGFX and it worked just fine. I migrated to stm32l442. I have copied the code for the flash driver, changed the lin...
Posted on April 03, 2018 at 00:53Hi guys,I have STEVAL-MKI183V1 connected to stm32l476rg NUCLEO. I have downloaded the C example code. Setup the SPI and the Interrupt pin using STM32CubeMX. With the help of some example code i hooked it all up. I ge...
Kudos from