cancel
Showing results for 
Search instead for 
Did you mean: 

Accelerometer MEMS in various ''accelerometer'' chips

Babip Bipbop
Associate II
Posted on April 26, 2018 at 17:17

Dear community,

I was just wondering if there was any way of knowing (or whether this is 'secret recipe') whether the very-MEMS within different chips are the same or not.

Namely, I would like to know whether I should expect the exact same behaviours from the LIS2DH and from the accelerometer part of the LSM6DSM.

Same for LIS2DH/LIS3DH for example... 

Any pointers to help me out ?

Thanks in advance, dear community

Best regards.

#mems #die #accelerometer
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Miroslav BATEK
ST Employee
Posted on May 02, 2018 at 22:08

You have to compare the datasheets, from them you can judge it the sensors are similar. But you will be able to only if the digital part is same or similar not the sensor element itself. There is no secret recipe.

LIS2DH and accelerometer part of LSM6DSM are competely different.

LIS2DH and LIS3DH are very similar.