MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Operating VL53L1x in histogram mode

Posted on March 14, 2018 at 19:31Dear all,We are interested in reading out time-of-flight histograms from the VL53L1X to explore the application potential for SPAD technology for medical and cosmetic mass-market applications. The device appears to h...

VL53L1x - gesture recognition

Posted on April 26, 2018 at 08:11Hi,Anyone know how to config VL53L1x to gesture recognition? In datasheet is information about support 1D gesture recognition, but nowere I cannot find information how to config it to gesture recognition and how to u...

Maximum cover window for VL53L1X/VL53L0X

Posted on March 28, 2018 at 16:07The previous proximity sensor VL53L0X has a application note (AN4907: VL53L0X ranging module cover window guidelines) that specifies the cover window thickness limits for different distances that can be measured.I wo...

Resolved! Which Sensor should I use?

Posted on April 08, 2018 at 08:59I need a sensor that is able to differentiate between distance 20mm and 23mm with no error.i.e. the accuracy and stability must be high (within 1mm only)which sensor should I use VL6180 or VL53L or something else?

smhhadima by Associate II
  • 1251 Views
  • 1 replies
  • 0 kudos

VL53L1 underwater use / experiences?

Posted on April 24, 2018 at 13:46I understand the older vl6180x works underwater, but I could not find any information regarding the VL53L1. Anyone tried it? If so, how well does it work?I'm looking mainly for proximity detection / distance measurem...

Resolved! What is the base address of the VL6180X registers?

Posted on April 25, 2018 at 21:56Looking at the data sheet for the VL6180X (p49-50), the registers are listed with their 'offset' address.Does this mean I have to add a base address to the offset addresses? If so, where is that found in the document...

gbarbour by Associate III
  • 987 Views
  • 2 replies
  • 0 kudos

Strange behaviour with LSM303DLHC

Posted on April 30, 2018 at 12:25I am seeing some curious behaviour with the LSM303DLHC sensor. I am using the magnetometer only, reading at 200Hz. My software responds to interrupts on the DRDY pin by reading six bytes starting from register OUT_X_...

Interrupt and FIFO settings in ISM330DLC

Posted on April 27, 2018 at 09:15Please tell me the details on Interrupt and FIFO settings in ISM330DLC. I need to store the Gyroscope and Accelerometer data into the FIFO . Please tell me what changes i need to do in kernel source code of ism330dlc...

shammi d by Associate II
  • 889 Views
  • 0 replies
  • 0 kudos

Resolved! LIS2DH12 excessive current draw

Posted on April 16, 2018 at 12:37I am using LIS2DH12 on my custom designed board for a BLE application. I noticed that the PCB had a huge current draw than expected and on further digging found the accelerometer to be drawing the excessive current w...