MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DS3 spi interface always gives low output

Posted on August 11, 2016 at 13:03I am working on STEVAL-MKI160V1 board which has LSM6DS3 sensor. I want to interface board to AARDVARK I2C/SPI adapter using which I can generate I2C/SPI signals to the sensor. I connected sensor board to adapter, us...

n239955 by Associate
  • 1715 Views
  • 3 replies
  • 0 kudos

How to configure a STM32CubeMX project for a STM32F769I-Disco board to use only the MEMS Mics and the out audio jack ?

Posted on July 06, 2018 at 18:19Hi, I am currently working on a STM32F769I disco board and I would like to create a minimalist project (i.e. I only want what is necessary to my project) I want to use the MEMS Mics to playback directly on the jack ou...

Resolved! LSM9DS1 Magnetometer Temperature Compensation

Posted on February 13, 2017 at 15:59What does the TEMP_COMP bit in CTRL_REG1_M of the magnetometer do?  Do the offsets need to be programmed for it to work?We are seeing up to 10 degree heading variations when moving the temperature from 10C to 30C,...

LIS3DSH Temperature Compensation

Posted on July 25, 2016 at 17:07Does anyone knows how the sensors sensitivity and offset changes over a big temperature difference?Application Note says:''TCSo - Sensitivity change vs. temperature: This parameter defines how sensitivitychanges with ...

bkamp9 by Associate
  • 1411 Views
  • 2 replies
  • 0 kudos

Is it possible to have several L3GD20H on the same SPI bus?

Posted on July 06, 2018 at 11:51Is it possible to have several L3GD20H on the same SPI bus (running SPI mode)?The datasheet says that if chip select is high the circuit goes to I2C mode.So by selecting one chip with chip select low and the other chi...

sima2 by Associate III
  • 836 Views
  • 1 replies
  • 0 kudos

Resolved! LIS3DSH Sensitivity

Posted on January 08, 2018 at 12:53Dear All,about this device I'm try to better understand the sensitivity parameters, from the datasheet, using the device at ±2.0g (FS bit set to 000) we must have a Sensitivity of 0.06 mg/digit, hence the number o...

FF1 by Associate III
  • 1586 Views
  • 3 replies
  • 0 kudos

LIS3DSH sample rate accuracy

Posted on January 29, 2018 at 21:55Hi there,Is there any spec on how accurate the sample rate of the LIS3DSH accelerometer is? In our application we configure the module to sample at 1600 Hz and apply to it vibration of a known frequency. However, a...

LIS3DH interrupts again

Posted on July 04, 2018 at 12:06I intend to use the LIS3DH as a very low power activity detector but have had no success in getting its interrupt output to behave in my application: I can make it stay always on or always off but never does it react ...

LIS3DSH Interfacing

Posted on July 05, 2018 at 06:32Hello,We are trying to interface LIS3DSH sensor to Raspberry Pi board through I2C. Is it possible to read the data from sensor without loosing any data if we have SCLK of 100kHZ and output data rate of 1600HZ?Please s...

Resolved! Setting LIS2MDL Interrupt Threshold

Posted on June 26, 2018 at 00:26Hi,I am trying to dynamically configure the interrupt threshold on the LIS2MDL. It seems that sometimes after setting a new threshold, the old threshold still is in effect and causes an interrupt transition on the out...