MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DH12 correct configuration for stream to FIFO

Hi, I need to get the FIFO contents prior to impact, to do this, I enable high pass, and go to stream to FIFO mode. But I get an interrupt as soon as I finish configuringI am configuring LIS2DH12 according to your application note:CTRL_REG1 = 0x37 //...

TNaru.10 by Associate
  • 902 Views
  • 1 replies
  • 0 kudos

LIS2DW12 resource request

I am wondering if you could provide any sample code for testing the LIS2DW12 on Arduino if you have any? Thanks!

JW.3 by Associate
  • 815 Views
  • 2 replies
  • 0 kudos

LSM6DSM fifo pattern error

I am using the FIFO to read both the ACC & GYRO data using the FIFO_DATA_OUT_H and FIFO_DATA_OUT_L at 52Hz ODR.But once every 1~2 hours, the FIFO data seems corrupted. Debugging it shows the FIFO Pattern number (FIFO_STATUS3 & FIFO_STATUS4) return a...

Resolved! LSM9DS1 side-effects of fast ODR setting?

I have been using the fast ODR setting to reach magnetometer data rates higher than 80hz. I have noticed that there are spikes of about +/- 250 in the data at higher frequencies. After some research, it seems this is caused by reading registers while...

ABoge by Associate II
  • 2385 Views
  • 5 replies
  • 0 kudos

LPS22HB PLE interrupt not working

Posted on July 15, 2018 at 05:18Hi I am working with the LPS22HB eval board from ST and trying to generate an interrupt when the pressure drops suddenly.  So according to the data sheet this would be a PLE event (2nd bit of 0x0B register) Below are ...

how to get lsm303c INT_XL interrupt be "active low"

Hi,I am trying to get lsm303c output an "active low" interrupt on pin INT_XL.here is my init code:void LSM303C_AccInit(void){    uint8_t result = 0;    ACCELERO_IO_Write(LSM303C_CTRL_REG1_A, 0b00100101);  // disable y axis to avoid mg     ACCELERO_IO...

GFone by Associate II
  • 1164 Views
  • 1 replies
  • 0 kudos