2018-08-15 7:50 AM
Hi,
I looking for ideal parameter for sound source localization for 2 microphones on-board, maybe someone testing this ? I tried to set different parameters for different algorithms and each time the angle print on the console was poorly reflected correct source sound location.
Maybe I should pay attention to the settings of other parameters if so which ?
libSoundSourceLoc_Handler_Instance.channel_number = 2;
libSoundSourceLoc_Handler_Instance.M12_distance = ???; //side or diagonal ?
libSoundSourceLoc_Handler_Instance.M34_distance = ???;
libSoundSourceLoc_Handler_Instance.sampling_frequency =
AUDIO_SAMPLING_FREQUENCY; //how value is the best ?
libSoundSourceLoc_Handler_Instance.algorithm = ACOUSTIC_SL_ALGORITHM_BMPH; //which algoritm better and why ?
libSoundSourceLoc_Handler_Instance.ptr_M1_channels = 2;
libSoundSourceLoc_Handler_Instance.ptr_M2_channels = 2;
libSoundSourceLoc_Handler_Instance.ptr_M3_channels = 1;
libSoundSourceLoc_Handler_Instance.ptr_M4_channels = 1;
libSoundSourceLoc_Handler_Instance.samples_to_process = 512; //how many samples
AcousticSL_getMemorySize(&libSoundSourceLoc_Handler_Instance);
libSoundSourceLoc_Handler_Instance.pInternalMemory = (uint32_t *) malloc(
libSoundSourceLoc_Handler_Instance.internal_memory_size);
error_value += AcousticSL_Init(&libSoundSourceLoc_Handler_Instance);
/*Setup Source Localization dynamic parameters*/
libSoundSourceLoc_Config_Instance.resolution = 5; // the best value is ?
libSoundSourceLoc_Config_Instance.threshold = 18;//the best value is ?
Thanks for every help