MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DSM fifo pattern error

I am using the FIFO to read both the ACC & GYRO data using the FIFO_DATA_OUT_H and FIFO_DATA_OUT_L at 52Hz ODR.But once every 1~2 hours, the FIFO data seems corrupted. Debugging it shows the FIFO Pattern number (FIFO_STATUS3 & FIFO_STATUS4) return a...

Resolved! LSM9DS1 side-effects of fast ODR setting?

I have been using the fast ODR setting to reach magnetometer data rates higher than 80hz. I have noticed that there are spikes of about +/- 250 in the data at higher frequencies. After some research, it seems this is caused by reading registers while...

ABoge by Associate II
  • 2378 Views
  • 5 replies
  • 0 kudos

LPS22HB PLE interrupt not working

Posted on July 15, 2018 at 05:18Hi I am working with the LPS22HB eval board from ST and trying to generate an interrupt when the pressure drops suddenly.  So according to the data sheet this would be a PLE event (2nd bit of 0x0B register) Below are ...

how to get lsm303c INT_XL interrupt be "active low"

Hi,I am trying to get lsm303c output an "active low" interrupt on pin INT_XL.here is my init code:void LSM303C_AccInit(void){    uint8_t result = 0;    ACCELERO_IO_Write(LSM303C_CTRL_REG1_A, 0b00100101);  // disable y axis to avoid mg     ACCELERO_IO...

GFone by Associate II
  • 1161 Views
  • 1 replies
  • 0 kudos

Gasket 3d model for VL53L0X . Where to download?

I'm trying to apply the VL53L0X to an project that require extra air gap between module and cover window. I just saw a video from YT: https://www.youtube.com/watch?v=puRvRsrfpTs that appear to be "official".There is 3d gasket model. It is available t...

DGodo by Associate
  • 817 Views
  • 0 replies
  • 0 kudos

VL53L1X Oudside

Posted on June 22, 2018 at 14:23I am looking for a successful setup for a VL53L1X in outside conditions any type of help to get more then 30 cm in sunny weather #vl53l1x

setting the VL53L1 ROI

Posted on July 09, 2018 at 13:01I'm tryong to set my ROI with the P-NUCLEO-53L1A1 and i can't find the function ( VL53L1_SetUserROI() ) in the SimpleRangingExamples Project , i'm using the IAR workbench , anyone have a clue ?