MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Typo in datasheet for LPS25H?

Hi.I wonder if it is possible to disable the I2c interface via CTRL REG2?in 7.7 in the datasheet it seems to be possible, but specification for bit 3 seems strange:[3] I²C enable (0: I2C enable;1: SPI disable)Is above this correct in the datasheet? i...

FFrid by Associate
  • 1309 Views
  • 2 replies
  • 0 kudos

TOF Sensor regarding

Hello sirGreetings !!!!!We have selected your TOF Sensor part number vl5l0x this sensor detect range 1.2 Meter in the White background but our requirement is TOF Sensor detect range in any color of the object up to 2 meters.so please share the TOF se...

hjani by Associate
  • 675 Views
  • 0 replies
  • 0 kudos

LIS2DE12TR: Trying to set up 4D/6D mode to trigger an interrupt

The datasheet for LIS2DE12TR is utterly confusing. It is missing any kind of flowchart for how the device operates in 4D/6D mode, or how to even set up registers correctly to enable these modes without conflict. Moreover, the registers are describ...

APast by Associate
  • 1144 Views
  • 1 replies
  • 0 kudos

LIS3DE reset w/o supply reset

We're using a LIS3DE in our project wired up to the MCU as following:So we're using I2C for communication and have access to both INT pins, but not to the reset line and neither is there a mechanism to hard-reset the accelerometer.During development ...

0690X000006BwSnQAK.png

Resolved! Any application software for STEVAL-WESU1 board

Posted on April 20, 2018 at 16:16Hello Experts,Recently I bought the STEVAL-WESU1 board and able to read the sensor data using android application.My requirement is to connect this wearable platform to other ARM board (raspberry pi board), raspberry...

LIS3DH Startup Sequence

Hi,This is my first question to the community so hello! :)I've recently started working with the LIS3DH accelerometer and I am experiencing some difficulty in interpreting the startup sequence for the device. Using the datasheet and AN3308 the startu...

Jono by Associate II
  • 2341 Views
  • 5 replies
  • 0 kudos

LIS2DH not functional on cold boot on our DRA726 arm boards.

When I first boot the board the accelerometer is not recognized in IIO. After a reboot it does or if I do a rmmod and then modprobe on the kernel modules.My kernel is based on the TI 4.4 kernel from the 3.02 automotive SDK. The accelerometer kernel m...

Michel C by Associate
  • 603 Views
  • 0 replies
  • 0 kudos

Problem with Lsm6dsl via i2c.

Hi! I have a custom pcb with Lsm6dsl connect to mcu (nrf52832) via i2c. I can write and read regs of Lsm6dsl well (who I am also return 0x6a). But when I try to write ODR bits in CTRL1_XL (10h) reg (for example 0x10) then I can not work,because it a...

DBelo by Associate
  • 657 Views
  • 0 replies
  • 0 kudos