2018-08-23 3:21 AM
Hi!
I have a custom pcb with Lsm6dsl connect to mcu (nrf52832) via i2c.
I can write and read regs of Lsm6dsl well (who I am also return 0x6a). But when I try to write ODR bits in CTRL1_XL (10h) reg (for example 0x10) then I can not work,because it alwaus return NACK (Negative Acknowledge).. like there is no i2c slave on this address.
If I write other bits in CTRL1_XL (10h) reg (for example 0x0f) it work OK.
Can anybody help me, what it is the problem?