MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB Device HS-IN-FS does NOT work

I am using STM32Cube_FW_F4_V1.21.0.This is very excellent software.UART,SPI,I2S,RTC,,,work fine but HS-IN-FS.I have checked HS and FS works fine.My target board is STM32469I-EVAL board and I'm using EWARM compiler suite.My application is USB_Device/M...

TKawa.17 by Associate
  • 789 Views
  • 0 replies
  • 0 kudos

VL53L0X Sensor Communication(Failed reach)

I bought vl53l0x sensor in mouser.I designed in my sensor board for my project. I refered in datasheet circuit.I added my board schematics.İn addition to ı constructed to ı2c level shifter with mosfet for the arduino communication but i did not answe...

LIS3DH Power-Down Mode

On my custom board LIS3DH is supplied with Vdd = Vdd_IO = 3.3 V and is driven through I2C digital interface.On power-on LIS3DH, after its boot sequence (5 ms) should be automatically configured in power-down mode with a current consumption less then ...

Vagni by Associate III
  • 2785 Views
  • 3 replies
  • 0 kudos

Range setting in ISM330DLC

Hi All,I am working on a project that is using ISM330DLC sensor for measuring the acceleration along the X,Y and Z-axis. When I set range 2G,4G and 8G I'm seeing difference in the sensor raw value and when I set it to 16G, I'm getting same data as 8G...

LSM6DSl edge-sensitive trigger mode

Hello,I want to use edge-sensitive trigger mode to synchronize multiple sensors. In the code snippet you can see the relevant code for that. The FIFO buffer doesn't get filled, even though I have a PWM as trigger on the INT2 pin. The low-pass filter ...

RHube by Associate
  • 1436 Views
  • 2 replies
  • 0 kudos

Can ST guarantee LIS2DH12TR never locks up

Hello,We are developing a product that has some circuitry permanently powered inside a sealed enclosure.We need to determine if we need a load switch for the host processor to cycle power to the LIS2DH12TR MEMs chip in the event that the MEMs chip lo...

YCohe by Associate II
  • 1040 Views
  • 1 replies
  • 0 kudos

Datasheet with Registers for VL53L1X

Hi togetherI'm working on a project for my study. I want to program a VL53L1X sensor. And I want to do it with I2C and setting different Register. But I can’t find a datasheet with all the registers.Can someone help me?

UStei by Associate II
  • 1529 Views
  • 1 replies
  • 2 kudos

LSM9DS1 driver init fail

Hi everyone,I am using a LSM9DS1 and the official driver: https://github.com/STMicroelectronics/STMems_Linux_Input_drivers/tree/linux-3.10.y-gh/drivers/input/misc/st/imu/lsm9ds1I have detected that occasionally the driver fails during the boot time:I...

0690X000006CKVtQAO.png 0690X000006CKWcQAO.png
Pastrana by Associate II
  • 943 Views
  • 0 replies
  • 0 kudos