User Activity

I'm trying to build example GPIO_IOWakeup with Keil IDE based on BlueNRG-1. I got this screen.What are the necessary steps to activate building and set up necessary parameters?I try with this activity:What to do? 
After creating new project in ST WiSE Studio the created folders and files are like in pictureWhen new project is compared with other projects from examplesit is noticed that some folders are missing.One of missing folder is User. In that folder the ...
I try to use STM32CubeIDE but I didn't find how to program, run and debugSPBTLE-1S and BlueNRG-M2 modules.I find that WISE Studio is more usefull. I try examples from BlueNRG-XNavigator. I find out that after activating BLE Beacon example module can ...
In my project I need to connect UART and I2C to BlueNRG-2 in module BlueNRG-M2. I need also to connect IO too.The inside module processor will manage functions.How I can program module processor? Can I use STM32CubeIDE?I also need to debug my code.
I'm designing project for Speed Control of 3-Phase Induction Motor with STGIPS30C60-H. I'm driving with microcontroler trough optocoupler. The motor is rotating in with desired speed about one minute and after stop. After that STGIPS30C60-H does not ...