MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ISM330DLC - question about SDx and SCx pins

Hello,I would like to ask a question related to ISM330DLC device. I am using in my application this device using I2C communication between STM32. During review I just realized that I didn't connect the SDX ( pin 2 ) and SCX ( pin 3 ) to VCC or GND (...

Need LIS3DH pin-compatible part that includes gyroscope

We've been successfully using the LIS3DH in its 3x3mm 16 pin package for a couple of years. Works great. But now this product requires gyro sensing too.What we need is a pin and package compatible Acc+Gyro so we can drop it onto the existing PCB and ...

Code for BME680 sensor

Hi guys,Does anyone have a working code for the BME680 interfaced with STM32. I have a code whose gas sensor component is not functional.

NSukh by Associate
  • 2025 Views
  • 2 replies
  • 0 kudos

Basic Functioning and UNICO

HiI am new to this lsm6dsoi am currently using STEVAL-MKI109V3 with STEVAL-MKI191V1 using unico.What i a getting is that "ADAPTER BOARD NOT SUPPORTED" I has also tried Serial Terminal still getting same result with *setdb191v1any help with this?

VBans.16 by Associate II
  • 1059 Views
  • 1 replies
  • 0 kudos

Problem with LIS3DH thresholds

Posted on September 02, 2017 at 13:08Hello allI have a problem with setting LIS3DH module to detect movement.To be more precise, I want the device to set the INT1 pin down when the it experiences 32mg acceleration change for 0.5 second. Here are my ...

Where to find the documentation of the VL53L1X registers?

Hi everyone, I do not post very often to ask for support but this time I really need help :smiling_face_with_halo: I am working with the VL53L1X (more precisely the Breakout boards which are really great). I successfully managed to get a distance val...