MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPS22HB PLE interrupt not working

Posted on July 15, 2018 at 05:18Hi I am working with the LPS22HB eval board from ST and trying to generate an interrupt when the pressure drops suddenly.  So according to the data sheet this would be a PLE event (2nd bit of 0x0B register) Below are ...

how to get lsm303c INT_XL interrupt be "active low"

Hi,I am trying to get lsm303c output an "active low" interrupt on pin INT_XL.here is my init code:void LSM303C_AccInit(void){    uint8_t result = 0;    ACCELERO_IO_Write(LSM303C_CTRL_REG1_A, 0b00100101);  // disable y axis to avoid mg     ACCELERO_IO...

GFone by Associate II
  • 656 Views
  • 1 replies
  • 0 kudos

Gasket 3d model for VL53L0X . Where to download?

I'm trying to apply the VL53L0X to an project that require extra air gap between module and cover window. I just saw a video from YT: https://www.youtube.com/watch?v=puRvRsrfpTs that appear to be "official".There is 3d gasket model. It is available t...

DGodo by Associate
  • 514 Views
  • 0 replies
  • 0 kudos

VL53L1X Oudside

Posted on June 22, 2018 at 14:23I am looking for a successful setup for a VL53L1X in outside conditions any type of help to get more then 30 cm in sunny weather #vl53l1x

setting the VL53L1 ROI

Posted on July 09, 2018 at 13:01I'm tryong to set my ROI with the P-NUCLEO-53L1A1 and i can't find the function ( VL53L1_SetUserROI() ) in the SimpleRangingExamples Project , i'm using the IAR workbench , anyone have a clue ?

Self-test LSM330DLC

Posted on February 07, 2014 at 09:25Hello,For a project we are using the LSM330DLC 3D accelerometer and 3D gyroscope module. Chapter 4.1. of the datasheet (Doc ID 022162 Rev 2) mentions self-test functionality, which can be enabled by setting the se...

m2 by Associate
  • 695 Views
  • 3 replies
  • 0 kudos

Library along with sensor fusion for LSM9DS1

We are planning to use 9DoF sensor LSM9DS1 with STM32L4 controller.We tried to find sensor library on web but not able to get one, can you pl provide us supported library including sensor fusion for STM controller?

LIS2DE12 temperature conversion

We have an LIS2DE12 accessed via i2c. We set:0x20 to 0x1f0x1f to 0xc00x23 to 0x80Then we read 0x07 until TDA is set.Finally, we read temperature data.Example 1:0x0c = 0x000x0d = 0x13Example 2:0x0c = 0x800x0d = 0xdfHow do we convert these values to d...

JPerr by Associate
  • 471 Views
  • 1 replies
  • 0 kudos

gyroscope calibration library for linux

Hi,We are using gyroscope calibration library for linux in order to get more accurate gyroscope values. Can u please tell me what value need to be set for the various parameters in the iNemoEngine_gbias_setKnobs() API .Thank you,Best Regards,Sharmi...

shammi d by Associate II
  • 672 Views
  • 2 replies
  • 0 kudos