MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Audio BSP missing in STM32L475VG (B-L475E-IOT01A)

Posted on April 04, 2018 at 15:32Hello everyone,Why is Audio BSP missing from the project? Please help me how to integrate it? Does anyone have an example code to make microphones (MP34DT01) working? or share experience how and where to start to mak...

vl6180x usage without library

Hi there, I have got quite an inaccurate range measurement result with vl6180x in my setup with stm8s003f3. I only use low-level I2C tx/rx communication and send to the slave address 0x52 start single ranging command 0x00;0x18;0x01 wait for 100mS and...

IKhly by Associate II
  • 606 Views
  • 1 replies
  • 0 kudos

STTS75 I2C No ACK from sensor

Hello ST Community,Long time lurker, first time poster.I'm having an issue with the STTS75 temperature sensor and I can't seem to figure this one out. Right now I'm just trying to pull the current sensed temperature from the chip; nothing fancy. I'v...

JD1 by Associate II
  • 1319 Views
  • 4 replies
  • 0 kudos

Resolved! What are the difference among operating modes in magnetometer of LIS3mdl in terms of the number of samples used to generate each output sample?

What are the difference among operating modes in magnetometer of LIS3mdl in terms of the number of samples used to generate each output sample?For example, I found that in ISM303DAC the number of samples used to generateoutput sample is four times le...

RTous by Associate
  • 655 Views
  • 1 replies
  • 0 kudos

High standby current of LIS3MDL

The static current of LIS3MDL is 0.2mA while the pin is connect to ground serial with 10K resistor, if this pin is floating, the current 0.07mA. The sensor is communication with Noridic nrf52 MCU via I2C. Please advise the appropriate connected for t...

AChan.5 by Associate
  • 717 Views
  • 3 replies
  • 0 kudos

VL6180X sampling rate and accuracy

I consider to use VL6180X sensor in a closed-loop system to measure a distance from the object. 1) I would like to sample distance measurement at 100-500 Hz. But if I read the manual correctly, even in continuous mode I can get measurements at best a...

AKhil by Associate
  • 597 Views
  • 0 replies
  • 0 kudos

Temperature Compensation LSM303C

Dear Sir / Madam,For our application there is a temperature range of -20 to +50 degrees celcius. However, over the complete range of temperature I would like the system to be within 0.1 degrees accurate. Due to the temperature drift in the sensor, th...

RLens by Associate II
  • 1796 Views
  • 7 replies
  • 0 kudos