MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Size and position of Hall Plates in IIS2MDC Magnetometer

HelloI want to use the IIS2MDC magnetometer in a device which measures magnetic fields that change rapidly as a function of position (e.g. fields with high gradients). For this purpose, I need to know two things which i couldn't find in the datasheet...

Dvon by Associate
  • 1259 Views
  • 1 replies
  • 0 kudos

On the IIS328DQ, are the INT pins active high or low?

I am assuming that since they can be configured as push-pull or open drain that they are likely active low, but I would like to confirm this assumption. It seems odd that there is nothing in the datasheet about these pins -- only info about their sof...

Resolved! MotionFX Library ARM Cortex-M4F Hardware Floating Point

Hi,I am attempting to port the MotionFX Library example to another processor. The project I am using as a reference is the DataLogFusion project for the STM32L476RG-Nucleo in the X-CUBE-MEMS1 V6.0.1. I am trying to compile it on another ARM Cortex M4...

Daniel L by Associate III
  • 2247 Views
  • 4 replies
  • 0 kudos

Impact of regular self test on MEMS.

Hello everyone, I'm developing an IoT product with the LIS3DH and I'm thinking about running the self-test regularly this could be anything between 30 minutes and 2 hours; would this kind of behavior impact the life of the sensor? is there any data o...

Out of range readings of VL53L1X

Though the maximum range of the VL53L1X is 400cm, it gives random readings within 400cm when it is directed to open space. The VL53L0X gives a value about 8.1m for out of range measurements so that we can filter out them. But in VL53L1X there is no w...

TSura by Associate
  • 10182 Views
  • 13 replies
  • 0 kudos

VL6180X Issues Interfacing with TI MSP432P401R Microcontroller

Hi all,I am trying to get the VL6180X to work with my TI MSP432P401R Microcontroller. I purchased my VL6180X on a breakout board manufactured by Adafruit (https://www.adafruit.com/product/3316). I have gotten it working with an Arduino just to verify...

PTran.9 by Associate
  • 998 Views
  • 1 replies
  • 1 kudos

LSM6DSM: Unreliable SPI

Hi all, I'm trying to bring up an LSM6DSM (MKI189 dev board) via SPI using a Nucleo and the STM C libraries for it. I've had some luck but I'm getting extremely unreliable SPI communication ( MISO line specifically ). For starters when I read the Who...

0690X000008AkLwQAK.png
Konami by Senior II
  • 2184 Views
  • 6 replies
  • 0 kudos