MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

lis2de12 pedometer

I am trying to use the lis2de12 as a activity level detector.By reading some posts here in the community I guess I need to setup HighPass filtering and a threshold so it gives interrupts everytime there is a movement bigger then a certain force.But I...

Mgeen by Associate
  • 1255 Views
  • 1 replies
  • 0 kudos

tranking cricket bat swing. with motion fx library.

I want to track the swing of cricket-bat using mems sensors. i'm running Motion FX library at 100hz and 200hz. motion fx library is failing some times to track the orientation if the swing speed is more . can I run MotionFx sensorfusion library at 30...

Testing LSM6MSOX without STEVAL-MKI109V3 evaluation board

Hi,i wanted to evaluate LSM6DSOX and for that i have ordered the breakout board STEVAL-MKI185V1 but not the STEVAL-MKI109V3 (mother board which interfaces with PC). i wanted to use the unico software to test the machine learning feature. is it possib...

Unknown type name 'sAcceleroParam_t', 'sTimeDomainAlarm_t', 'sAcceleroParam_t', 'sTimeDomainAlarm_t', 'sAcceleroParam_t', 'sAxesMagResults_t' and 'sFreqDomainAlarm_t'

<command-line>:0:0: note: this is the location of the previous definition  In file included from ../Src/TargetPlatform.c:40:0:  ../Inc/sensor_service.h:74:37: error: unknown type name 'sAcceleroParam_t'  extern tBleStatus TimeDomain_Update(sAccelero...

0690X00000981LgQAI.png

.

FPira by Associate
  • 606 Views
  • 0 replies
  • 0 kudos

Trouble getting sensortile working with small cradle

Not sure if I'm in the right place for this question, but I recently started using the sensortile development kit for a class/project. I've done all the tutorials with the sensor mounted to the expansion cable. However, now my project requires the ...

JCrow by Associate II
  • 2083 Views
  • 5 replies
  • 0 kudos