MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to use the X-CUBE-MEMS1 for SensorTile

So I wanted to use the X-CUBE-MEMS1 library for the SensorTile module but noticed that the projects were made for the IKS01A1 and the IKS01A2 boards. Which one of these projects/boards would I need to select for the SensorTile application?

VRao.1 by Associate III
  • 1291 Views
  • 1 replies
  • 0 kudos

Camera module

selam4 kamera ile ayrı ayrı fotoğraf çekmek ve gözden geçirmek SD karta istiyorum istiyorum. Kameralar ve işlemci arasında 3 metre mesafe olacak. Bu mesafe görüntü çekmek için uygun mu? bunu nasıl yapabilirim. Sccb protokolü bunu destekliyor mu yoksa...

HTosu.1 by Associate
  • 931 Views
  • 2 replies
  • 0 kudos

Hi, I am using LSM303AGR for both Compass and Accelerometer with the I2C interface. I read the datasheet but I want to double-check about connection.

As I read from data-sheet, for I2C interface, I need to connect CS_XL & CS_MAG to VDD. Do I need to connect them to Digital Pins to able to switch between Accelerometer and Compass. Could you please check my schematic and confirm is it correct to use...

SSert.1 by Associate
  • 1129 Views
  • 1 replies
  • 0 kudos

LSM303AGR calibration & accuracy

Hi,​We have tested our custom LSM303AGR board with MC and EC Libraries that ST provides. We see that our degree calculations accuracy is within +/- 4 degree. That is, we have degree which has deviation of 4 degree when it is stationary. We see that w...

AAYKA.1 by Associate II
  • 1869 Views
  • 2 replies
  • 0 kudos

Problem with Bluecoin and echo cancellation

Hy,I'm trying to do some tests on echo suppression using evaluation boards BlueCoin and CoinStation.The software I use is the one provided by ST to interact with BlueCoin that is, FP-"AUD-SMARTMIC1 GUI.exe" in addition to theaudacity.exe program.As s...

apenn.13 by Associate II
  • 1821 Views
  • 4 replies
  • 0 kudos

Must LPS25HB reserved pin 3 be grounded?

Pin 3 which is reserved should be grounded according to the data sheet but was left floating on our boards. May this be the cause of SPI issues? Regardless of what we read or write, we see LPS25HB output 0xff11 on SDO. LPS25HB outputs data on fallin...

MStro.1 by Associate
  • 1374 Views
  • 3 replies
  • 0 kudos

How can I connect STEVAL-MKI207V1 over I2C, with Ti LaunchPad?

Hello ST Community Experts,I am completely beginner here. We have purchased STEVAL-MKI207V1 for Accelerometer, Ti MSP432 as MCU. We wanted to connect both over I2C. But facing some problems.STEVAL-MKI207V1 Kit has ISM330DHCX sensor. I checked datashe...

HarshC by Associate
  • 1652 Views
  • 2 replies
  • 1 kudos

STEVAL MKI109V3 Unable to enter DFU

Hello I have installed Unico and DFUSE DEMO and all the drivers, and when I connect my board to the PC I can see the virtual com port 6:but when I open dfusedemo, and press button 3 and 2 together then release 3 then 2, I get this:I can't get the S...

0690X00000DYV4nQAH.png 0690X00000DYV57QAH.png
WGeng.1 by Associate II
  • 1542 Views
  • 2 replies
  • 0 kudos

www.st.com

Dear community,I found the Q&A but I can't find the place where I can write my own question. So I do it here for now.I have a question about the vl53l0x api. In the API manual they say that you should call it in this sequence:dataInit()staticInit()Pe...

Rvalk.1 by Associate
  • 718 Views
  • 0 replies
  • 0 kudos