MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi, I have MB1329B module with quectel BG96 with firmware version: BG96MAR02A06M1G. I intend to send data by NB-IoT with a plastic sim card but it isn't working because the SIM is not detected.

I have the PWR enable pin at high level, the sim_select1 pin also at high level and the sim_select0 pin at low level (because I have a plastic sim).I'm sending the following AT Commands using usb connection directly between the module and a computer:...

FCelm.1 by Associate II
  • 2885 Views
  • 5 replies
  • 0 kudos

Resolved! Minimum range VL053L0

I searched in the datasheet, but I could not find any information about the minimum possible measuring range. There are only values for the maximum range.Is there any official information from ST available?What are your experiences?Thanks in advice f...

GPrit.1 by Associate
  • 1281 Views
  • 4 replies
  • 0 kudos

Resolved! LSM6DSO interface with MCU : Generation of wakeup/activity/single tap interrupt during double tap. Expected : Only double tap. Actual: wakeup/activity/single tap interrupts also along with double tap interrupt

Issue Summary:Generation of wakeup/activity/single tap interrupt during double tap.Expected : Only double tap.Actual: wakeup/activity/single tap interrupts also along with double tap interruptplease find the below Analysis for your reference. Registe...

srao.1 by Associate II
  • 3276 Views
  • 7 replies
  • 0 kudos

Resolved! Can I leave SDO_A/G pin floating on the LSM9DS1?

Does it have internal pull-up? Or do I need to connect that to a pin? Is there a way to "burn" the i2c address?I'm asking as I have a design where I left that pin open. On some devices I have I2C communication issues, and I am asking myself if they c...

TWied.1 by Associate
  • 1396 Views
  • 2 replies
  • 0 kudos

Sensortile.box seems to be stuck

Hello,​I​ got today a ST.box, and I was starting to play around trying different demos through the basic mode.I had initially a long firmware update.Then at the third demo I tried to upload the Blue led got stuck, and the​ ST.box is no more respondin...

MGran.2 by Associate
  • 2198 Views
  • 7 replies
  • 0 kudos

Accelerometer z-axis on LSM6DSM jumps too much!

I am using an LSM6DSM but I got weird data on the z-axis for the accelerometer, as you can see in the attached picture z-axis jump too much in comparison with other axises, the device was steady in the whole sampling time.So does anybody have any ide...

Nta by Associate
  • 1458 Views
  • 3 replies
  • 0 kudos