MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LPS33HW Temperature absolute accuracy

Temperature absolute accuracy. This parameter was not found in the datasheet.Of the 15 sensors tested, the temperature ​difference was 5 degrees.What ​temperature absolute accuracy should be?

PSoko.1 by Associate II
  • 1647 Views
  • 5 replies
  • 0 kudos

I tried to install the GUI en.STSW-IMG004 to run my EvalBoard with VL53L1x. But the insatllation end with Error Massage 1721.

Hello everybody,I tried to install the GUI en.STSW-IMG004 to run my EvalBoard with VL53L1x. But the insatllation end with Error Massage 1721 (see attached). I ried it also on a second Hardware with the same result. What did I make wrong? Regards Dani...

DPalm.1 by Associate
  • 1543 Views
  • 4 replies
  • 0 kudos

How to detect angular movement and wake up LIS2DW12

Hi, I have an LIS2DW12 fitted to a STEVAL-MKI179V1 board. I have it connected to a microcontroller programmed to set an interrupt pin on wake up as per DT0098. The interrupt pin goes high with a light tap in the xy or z axis. However I want it to det...

DSqui by Associate II
  • 2083 Views
  • 5 replies
  • 0 kudos

VL53L1X People Counting ROI center

I am implementing an “auto calibration�? of the ROI in my people counting algorithm based on the one provided by ST. The program defines the centers of the two zones used to detect entry/exit in an area. Currently I run a simple detection algorithm t...

HMull.1 by Associate II
  • 1272 Views
  • 3 replies
  • 0 kudos