MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LIS2DE12 Vdd and VddIO power path

Hello,I'm developing an ultra-low-power circuit with LIS2DE12. I would like to have the accelerometer running with IRQ enabled, but serial communication shutted down.I can't understand at whitch power path the INT1 and INT2 are connected (Vdd or VddI...

Is there a IOC file for SensorTile example projects?

I am evaluating MEMS sensors using the SensorTile hardware and accompanying software (STSW-STLKT01). The toolkit has thus far been very nice. In order to move the project further I now want to port the AudioLoop example project to another MCU on a Nu...

Resistor changes for STEVAL-MKI196V1 and STEVAL-MKI109V2

Hi,On the MKI196V1 webpage (https://www.st.com/en/evaluation-tools/steval-mki196v1.html) It says that:"Changing the resistor settings is also compatible with the STEVAL-MKI109V2 motherboard"I cannot find any documentation on which resistor changes ar...

0693W000006EONBQA4.png
MSack.1 by Associate
  • 901 Views
  • 1 replies
  • 0 kudos