MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

WHO_AM_I issue in ASM330LHH

I am using the ASM330LHH connected to the processor via 4-wire SPI communication. I’m trying to read the WHO_AM_I register, which should return 0x6B according to the datasheet, but I keep getting 0xFF. The CS line is set correctly before and after th...

Jigs by Associate
  • 711 Views
  • 2 replies
  • 1 kudos

Resolved! ASM330LHH ODR and FS operating procedures.

Can I operate ODR_XL[3:0], FS[1:0]_XL and LPF2_XL_EN of CTRL1_XL of ASM330LHH simultaneously?Should I set FS[1:0]_XL and LPF2_XL_EN first and then set ODR_XL[3:0]?

ggob by Associate III
  • 701 Views
  • 1 replies
  • 0 kudos

LSM303AGR Application Note Clarification Needed

Hello everyone, I am currently using the LSM303AGR's magnetometer and accelerometer. After coding the self-test procedure from the datasheet, and noticed that the number of samples for the magnetometer self-test is way higher than the number of sampl...

LIS3DH Self Test output change too low

Hello,i am trying to run the self test procedure on the lis3dh according to Application Note 3308 but for some reason the  output change (13 lsb) is below the minimum value listed in the lis3dh (17lsb) .If i run the procedure multiple times in a row ...

kweikamp by Associate
  • 769 Views
  • 1 replies
  • 0 kudos

Resolved! LPF filter on IIS2ICLX inclinometer

I would like to implement a low pass filter to filter out noise at frequencies above 2Hz on the IIS2ICLX inclinometer. I would like to have as high an ODR as possible, let's assume 833Hz. My signal has a low frequency, around 0.5Hz.LPF1 will clearly ...

Resolved! ASM330LHH TDA bit not set to 1?

If the TDA bit is not set to “1” even once after 400ms has passed after the sensor is turned on, is it likely that the startup has failed?

ggob by Associate III
  • 819 Views
  • 3 replies
  • 0 kudos

LSM6DSOX MLC issue

I am using the MLC of the LSM6DSOX along with the Nucleo-L432KC. I am using the .h file generated from the examples provided by ST (STMems_Machine_Learning_Core\application_examples\lsm6dsox\Motion_intensity\lsm6dsox_motion_intensity).uint8_t LSM6DSO...

Bassem54 by Associate
  • 730 Views
  • 0 replies
  • 0 kudos

Resolved! Need confirmation MSL level MPN - LIS2DW12TR

Hi Expert, Good day. Refer to the attached label image. One label shows MSL 1 and the other shows MSL 3 for MPN LIS2DW12TR. However, the Reliability Evaluation Report for this P/N indicates MSL 1. Both labels have the same COO but different MSL level...