MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Data rate vs Data reading rate in mems sensors

Hi,I am configuring the mems sensor data rate as 30hz,So what should be the data reading rate in this case. I mean is it necessary to put a delay after configuring the sensor for reading data continously Or we have to check the status of data ready...

Interfacing with onboard i3g4250d gyroscope on STM32F429i

I have been trying to test and get the gyroscope to communicate via SPI for a bit however it just seems to *refuse* to respond. As per the User manual for the board UM1670, PC1 is CS, PF7 is the serial clock, PF8 is MISO, and PF9 is MOSI all for SPI5...

SAgaz.1 by Associate II
  • 3723 Views
  • 2 replies
  • 0 kudos

The marking information of LIS2DHTR

HI sir, we have received the item marking show 702, may i ask you what is it represent since we can't find the marking information from the spec. sheet., thanks.

VICTOR1 by Associate II
  • 2835 Views
  • 3 replies
  • 0 kudos

Resolved! AIS1120SX/AIS2120SX Tips and Suggestions

I'm in the process of some development using ST's AIS1120SX Accelerometer, in conjunction with a Nucleo L432-KC development board. I thought I would share some tips and suggestions I have about the accelerometer, as I found it particularly difficult ...

CJeff.1 by Associate
  • 2266 Views
  • 3 replies
  • 1 kudos

Resolved! How do you use the .ucf file generated by the UNICO GUI and why do the outputs seem to make no sense, comparing it to the register description found in the data sheet?

I am working with the Sensortile.Box right now. More specifically, I want to configure the pedometer function with the MLC to work with certain configurations. The accelerometer has to be set to 16g Full Scale, because of a fall-detection functionali...

KWern.1 by Associate II
  • 6121 Views
  • 6 replies
  • 0 kudos

LIS2DH12 init problem for FIFO stream mode

Hi Everybody,I have a weird problem initializing LIS2DH12 in FIFO stream mode with the official ST driver. This is my initialization code:bool lis2dh12wInit(lis2dh12w_cfg_t *cfg) { uint8_t whoamI; lis2dh12_ctrl_reg3_t ctrl_reg3;   /* set read a...

LIS2DH12 reset (BOOT in CTRL_REG5)

Hallo,I am wondering how can I reset the LIS2DH12 accelerometer. I am using the official ST driver which preserves register contents on nearly all actions (read-modify-write), and the MCU in hardware may perform a soft reset when it tries to re-initi...