MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DW12 temperature reading fluctuates

Hi,I have created a small function that reads out the 8-bit temperature register in the lis2dw12 sensor. The code is shown belowstatus lis2dw12::temperature(int8_t *temp) { *temp = static_cast<int8_t>(read_reg(REG_OUT_T)) + 25; printf("%d\r...

0693W00000DmdcgQAB.png
CThue.1 by Associate II
  • 1755 Views
  • 1 replies
  • 0 kudos

LIS3DH - Cannot have position detection running properly

My LIS3DH is embedded on a PCB with gravity on Zh (upside down).It is configured with:ODR 10Hz, Z axis enabledNo filterFS @2HzIA1 on INT1Interrupt active HIGHAOI and 6D pos (for position detection)INT1 threshold set to 0x39 (around 0.916g)This config...

SChab.1 by Associate II
  • 3310 Views
  • 6 replies
  • 0 kudos

Resolved! ‎LSM6DSLTR‎ Threshold event

Hi! I’m using the ‎LSM6DSLTR‎, and really just need to trigger an interrupt whenever the device rotates at a speed greater or equal to a given threshold. Do I need to set up any FIFO data, or is there a way to only generate an interrupt based on a ro...

BMitchen by Associate
  • 2132 Views
  • 2 replies
  • 0 kudos

Resolved! Use of DRDY_M & DEN_A/G in LSM9DS1?

I am trying to build custom boards using LSM9DS1, I shot through the data sheet, but the information on these two pins is not clear enough? What is the purpose of these pins(DRDY_M & DEN_A/G)?

VKoga.1 by Associate II
  • 3807 Views
  • 6 replies
  • 0 kudos

Resolved! For the IIS3dWB ODR and sampling rate...

I need to confirm what the ODR represents - the default ODR is 26667Hz. But what is the actual internal sample rate pre anti-aliasing filter (which must be implemented internally)?Assuming the actual Fsample is at least 26667, then ODR simply represe...

ESpen.1 by Associate
  • 2170 Views
  • 2 replies
  • 1 kudos

Resolved! How to Synchronize multiple LSM6DSOs

Hello fellow ST guys. I'm working with the LSM6DSO IMUs in my project. Nice chip indeed. Now I need to connect multiple IMUs and I need to synchronize them, so that I can read the data from all of those chips sequentially (asserting chip select pins...

Pajaka by Associate III
  • 1757 Views
  • 1 replies
  • 0 kudos

SensorTileBox SL-MKSBOX1V1 - Cloud and MQTT

Hi I have four questions please: 1- is there a new version of the UM2499 pdf manual, as most of the links are broken ? 2- I get this error with IBM watson IoT quickstart - (kCFErrorDomainCFNetwork error 2), i get this in different Iphones. As i thoug...

Hjawa.1 by Associate II
  • 1969 Views
  • 3 replies
  • 0 kudos

ST_ sensors driver linux BIG PROBLEM

I have an embedded platform AT91SAM9260 based running on a buildroot based Linux with kernel 4.19.78-linux4sam-6.2 which includes an LSM6DSO and a LIS2MDLTR as well.When st_* drivers are loaded all communications via i2c is returning EBUSY and even ...

PRegn.1 by Associate II
  • 2827 Views
  • 6 replies
  • 0 kudos