MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Sensortile.box: How to program? Battery life?

I'm working on a Sensortile.box for the first time. I'd like to create an app that records steps, activity type, and axis information (gyro) for three days straight. Would appreciate any insight for a newbie here. Questions below: I'm working on a Se...

VL53L0X Register Map?

Posted on June 13, 2016 at 21:32Having previously used with the VL6180X, I expected the VL53L0X to be similar in architecture.  However, while I found a somewhat useful data sheet, it does not seem to contain a register map.  It seems I'm supposed t...

wayne23 by Associate
  • 13487 Views
  • 16 replies
  • 2 kudos

Resolved! LIS2DH12 16G full scale goes up to 24G?

Hi, this is a question about LIS2DH12. I've been puzzled over the full scale settings for this sensor.As it says in the datasheet, the ranges are ±2g/±4g/±8g/±16g, yet when I am set at 16g, I am able to obtain a max range of -24656, +24384.I am using...

IC.1 by Associate II
  • 1563 Views
  • 1 replies
  • 0 kudos

Resolved! LIS2DE12TR

Hello,May I get some document information for parts marking of PN#LIS2DE12TR?The label mark say is A2L 2D? Is it right? Have any document for the marking?Thanks

Manman by Associate III
  • 3954 Views
  • 3 replies
  • 0 kudos

Question about MotionFX error in 9-axis

Hello,I'm currently working on a project requiring to get X, Y and Z angles from 2 sensors, (IIS2MDC and ISM330DHCX). In order to do so, I use MotionFX and its 2 functions, MotionFX_propagate and MotionFX_update, both used to run Kalman STM's algori...

MPoul.2 by Associate II
  • 16622 Views
  • 29 replies
  • 0 kudos