Skip to main content
JRaim.1
Associate
January 19, 2022
Solved

Hello, I am working with H3LIS331DLTR elements, I can not decipher the marking, can you help?

  • January 19, 2022
  • 3 replies
  • 2609 views

..

This topic has been closed for replies.
Best answer by Eleon BORLINI

Hi @JRaim.1​ ,

In addition to Peter's complete description, we can say the third line, and especially the two last letters/numbers, refer to the specific assembly lot of those samples.

This information is useful at failure analysis level.

-Eleon

3 replies

Peter BENSCH
ST Technical Moderator
January 19, 2022

Welcome, @JRaim.1​, to the community!

the important marking is H3D3, which stands for H3LIS331DLTR.

The first and last lines should only be required if a quality issue arises and the component would need to be examined in detail. Maybe the datecode here is interesting: line 1, 830 = year 2018, week 30.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
JRaim.1
JRaim.1Author
Associate
January 19, 2022

Our quality engineers have encountered some problems in identifying the markings.

We would be very grateful if you could explain the meaning of the symbols (line 3) in the attached photo. Is it a data code or a lot number? How can one packing tape contain devices with different markings?

Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
January 21, 2022

Hi @JRaim.1​ ,

In addition to Peter's complete description, we can say the third line, and especially the two last letters/numbers, refer to the specific assembly lot of those samples.

This information is useful at failure analysis level.

-Eleon