MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! If the electrode is embedded in an insulator, isn't the sensing process dielectric polarization rather than electrostatic induction?

If the electrode is embedded in an insulator, isn't the sensing process dielectric polarization rather than electrostatic induction?The following text is quoted from 「Application Note "Qvar sensing" (AN5755) p2.「 A signal is derived from the electron...

Shion by Associate II
  • 284 Views
  • 2 replies
  • 1 kudos

Resolved! ASM330lhh Latency

Hello Everyone, Have anyone measured the latency from sensing the physical motion to the output of the sensor? I couldn't find in the datasheet how much time the filters takes. Thanks

majellan by Associate
  • 277 Views
  • 1 replies
  • 0 kudos

LSM6DSO32 Pedometer Returns 0

Hi There, I've designed a board which uses a LSM6DSO32 sensor over i2c for accelerometer, gyro and it's embedded pedometer function. I've been able to reliably get data from the sensors accelerometer and gyro registers however I've not been able to g...

LIS2DU12 Self-Test Not Producing Expected Deviation

Hello, I’m using the LIS2DU12 accelerometer and trying to perform the positive self-test exactly as described in the official application note. However, I’m consistently seeing results that do not meet the expected deviation thresholds, and the self-...

Resolved! MSL of accelerometer sensor

Hi,Where can I find inforamtion on Moisture sensitivity level for each sensors? I checked datasheets and few other documents in the product page but couldn't find it. I want to know the MSL of IIS3DWB.Best regards,Kev

KJose.1 by Associate III
  • 228 Views
  • 1 replies
  • 1 kudos

Serial (COM) Port for reading IMU data from STEVAL-MKI109D

Dear all,I would be interested to use a MKI109D dev board (with USB C connector) to stream data from a MKI178V2 board fitted with a SM6DSL IMU sensor to a preferably a python or cpp based script using something like a pyserial library. I have tested ...

SaeidD by Associate
  • 357 Views
  • 1 replies
  • 0 kudos

STM32nucleo embedded STLINK for sensortile.box

Hi, i have a question, is it possible to use the embedded STLINK on the nucleo-f446re for programming the sensortile.box (steval-mksbox1v1) ? If so, how do i have to connects the pin? I have a JTAG Adapter v1.0 (included in the sensortile box), so i'...

alemezz by Associate
  • 264 Views
  • 1 replies
  • 0 kudos

LPS22 sensor suddenly behaving weird

I've had this problem with an ILPS22QS and now I'm having it with an LPS22HH. It has me completely mystified. The issue is like this: The pressure sensor works as normal for a week or even multiple weeks and then all of a sudden it enters a mode wher...

weird-behaving-pressure-sensor.png
mbenkmann by Associate II
  • 1659 Views
  • 5 replies
  • 0 kudos