cancel
Showing results for 
Search instead for 
Did you mean: 

If the electrode is embedded in an insulator, isn't the sensing process dielectric polarization rather than electrostatic induction?

Shion
Associate II

If the electrode is embedded in an insulator, isn't the sensing process dielectric polarization rather than electrostatic induction?

The following text is quoted from 「Application Note "Qvar sensing" (AN5755) p2.

「 A signal is derived from the electronic circuit due to the fluctuations in the electric field resulting from the passage of the charged particles. If the electrode is embedded in an insulator or there is no direct contact between the electrode and the particles, the sensing process is achieved through electrostatic induction. 」



1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @Shion ,

When the electrode is embedded in an insulator, the sensing process at the electrode is primarily electrostatic induction, but it is strongly influenced by dielectric polarization of the surrounding insulator.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Federica Bossi
ST Employee

Hi @Shion ,

When the electrode is embedded in an insulator, the sensing process at the electrode is primarily electrostatic induction, but it is strongly influenced by dielectric polarization of the surrounding insulator.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi @Federica Bossi

Thank you for your comment. That being said, it was so. Is there a document that explains in detail the physical principles of this sensing? If so, I would appreciate it if you could let me know.