MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

high current consumption for LIS2DTW12

I used the LIS2DTW12 adapter board (STEVAL-MKI190V1) with I2C communication. power supply: 3VWith low power mode 12.5Hz, the current consumption is normal as 1.3uA (datasheet 1uA). But when it's set as 12.5 Hz, high performance with low noise mode, t...

0693W00000LzPKvQAN.jpg
lgu.1 by Associate
  • 677 Views
  • 0 replies
  • 0 kudos

MotionFX output used for dead reckoning

We are trying to use data from MotionFX output in order to do dead reckoning.We are using linear acceleration which is as per our understanding equal to:acceleration - gravity accelerationLinear acceleration is being integrated in order to get veloci...

0693W00000KcTuYQAV.png
AMahm.2 by Associate
  • 1711 Views
  • 2 replies
  • 0 kudos

Inferencing with Microphone

I have stm32f746 discovery board. I need to get input by microphone, and give it to my tensorflow model. I could find neither a plain documentation nor a video. Can you please inform me how to work with microphone on STM32?Thx for your responses.

I'm using the ST iis3dwb mems accelerometer and I'm trying to configure it to use the internal FIFO and generate the interrupt lines INT1 or INT2, but they aren't firing. What am I doing wrong?

I'm using the STM32-F446RE Nucleo board. I am using PB1 and PB2 to trigger on the iis3dwb interrupts; PB1 and PB2 are setup as GPIO_EXTI1 and GPIO_EXTI2 respectively. These interrupts work as I have a breakpoint in the interrupt handler's and can tri...

PJamr.1 by Associate
  • 1229 Views
  • 0 replies
  • 0 kudos

Reading stale data from LIS2DE12

We are currently implementing a LIS2DE12 accelerometer into a project, but we have issues where they sometimes get "stuck" and continue reporting back the exact same values from when it was in motion.Current implementation uses 1hz refresh-rate, usin...

patric by Associate
  • 873 Views
  • 0 replies
  • 0 kudos

Very strange power profile on LSM6DSL

Good morning.We are testing several motion sensors for a commercial medical wristband. We have selected the LSM6DSL to evaluate its suitability. However, we have detected a very strange power consumption pattern. The VCC pin consumes as expected an a...

0693W00000LwZR7QAN.png 0693W00000LwZRHQA3.png
gutzchi by Associate II
  • 1954 Views
  • 3 replies
  • 0 kudos