MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Is X-CUBE-MEMS1 supported on STM32N6

So i'm trying to install X-CUBE-MEMS1 in the IOC file of a STM32N6-DK board.  The problem i can't seem to install it?  All the tabs are greyed out and have little red cpu marks by them.  Is X-CUBE-MEMS1 supported on STM32N6 processors?   When i go to...

Screenshot from 2025-11-17 12-20-46.png

FIFO data in Stream-to-FIFO mode

Hi,It's mentioned in the datasheet that the sensor will convert the FIFO from streaming (reading data all the time) into FIFO (holding the data until it's read) If i am getting it right, then my question isWhen exactly will the sensor read ? Will it ...

abduuu by Associate II
  • 400 Views
  • 2 replies
  • 0 kudos

Sensing total acceleration LIS2DH12

I was asking can I sense (generate interrupt) over the overall acceleration ?Because in the datasheet it was mentioned that I can manipulate the interrupt between X, Y, Z high and low.But it'd be helpful for me if I can generate an interrupt based on...

abduuu by Associate II
  • 303 Views
  • 1 replies
  • 1 kudos

Resolved! What are the benefits of sensor hub

Parts i'm looking to connect * STM32N6 - microcontroller * LSM6DSV320X -  Master Sensor IMU * LIS2MDL - On sensor hub Magnetometer     Question - is there any benefit to connecting the IMU master sensor to the LIS2MDL on the sensor hub vs connecting ...

LSM6DSV16X does not generate INT1 interrupt.

Hello.I am using an STM32H562VI board with an LSM6DSV16X sensor,and when I read the whoami value, it reads as 71.I configured the register as follows to check the interrupt on INT1./* Enable Block Data Update */ lsm6dsv16x_block_data_update_set(&dev_...

LSM6DSV16X .jpg LSM6DSV32X.jpg
heesu by Associate
  • 567 Views
  • 2 replies
  • 0 kudos

Resolved! ST1VAFE3BX 50/60Hz notch filter?

In application note TN1571 "Reference design based on the ST1VAFE6AX and ST1VAFE3BX biosensors..." Table 2 mentions that ST1VAFE3BX has a selectable 50/60Hz notch filter. However, there's no further reference to this filter or how to enable it in the...

bwilkins_0-1762888975471.png
bwilkins by Associate II
  • 440 Views
  • 2 replies
  • 0 kudos

Resolved! LIS2HH12 not responding

Hello,I have the LIS2HH12 chip in two separate boards, same board, same firmware.  These devices have been working well, producing X,Y,Z data.  Until today, that is, after a firmware update.This device is the only thing on the I2C bus, 100KHz, 5.1K p...

2025-11-07_223312.jpg 2025-11-07_223345.jpg
JonFick by Associate
  • 534 Views
  • 2 replies
  • 0 kudos